Part Number: UCC27301A Other Parts Discussed in Thread: UCC27302A Hi team,
Does UCC27301A all package include bootstrap diode?
Because I saw the VSON layout exsamples add internal diose.
Part Number: UCC27301A Other Parts Discussed in Thread: UCC27614 Hi team,
The customer wants to calculate whether the minimum drive current value can be provided under the most stringent conditions. thansk
Part Number: UCC27301A Hi TI Teams,
Now I using the UCC27301A for 48V system BLDC. Measure the low-side mosfet VDS when the load transients. If the high-side mosfet switches off the VHS voltage gose negtive(max negtive voltage is -6V and the pulse width…
Part Number: UCC27301A Hi team,
Could you give some suggestion why high side Vgs lower low side Vgs?
CH2 is Ho , CH3 is Lo , I think 12V-0.7(V)=11.3V Ho is normal.
Part Number: UCC27301A-Q1 Are the DDA (SOIC) and DRC (VSON) packages for the UCC27301A-Q1 using the same silicon?
I noticed that the DDA package does not feature an EN (enable) pin and was wondering if the tieing of that pin was done with a different…
Part Number: UCC27301A-Q1 How do the HO and LO outputs of the UCC27301A-Q1 behave when the device's VDD pins is at ~0V (unpowered) and connected FETS are powered with a high voltage? For example:
Is there any risk to the UCC27301A-Q1?
If HO and…
Part Number: UCC27301A Other Parts Discussed in Thread: UCC25800 , SN6505B Tool/software: Hi Team,
Do we have analog control integrated half-bridge driver? Similar with IFX AUIR2085S. UCC27301A need an external control.
I also discuss with customer…
Part Number: UCC27301A-Q1 Other Parts Discussed in Thread: UCC27201A , , UCC27201A-Q1 Hi,
I'm considering using the #-Q1 (HSOIC (DDA) package) in our next design.
Since the spec is preliminary, I would like to know if I could rely on the following…
Part Number: UCC27301A Tool/software: Hello team,
Is it okay to add external bootstrap diode to UCC27301A? (Like on the figure below.)
I know there is internal diode, but my customer want more current to the bootstrap capacitor.
Best Regards,…
Other Parts Discussed in Thread: UCC27301A-Q1 Tool/software: Hi TI team,
I do not want to use the resistor and diode integrated in UCC27301A-Q1, so I h a ve a dd ed a n exte r nal r esistor and diode.
Can you guide me in calculat ing th e charging…