Hello,
The UVLO detection logic controls the driver output stage so at the point of UVLO falling detection, the output will be driven low with the same drive current during UVLO as when in normal operation.
Regarding your second question, yes you…
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27284-Q1 , UCC27311A-Q1 Tool/software: Hi Team,
This is FAE Jayden, My customer would like to know do we have a device which has the same package with UCC27282Q1 but without interlock function…
Hey Gary,
Thank you for reaching out with your questions regarding the UCC27531.
The UCC27531 can be used as a high-side driver and there are a few ways to do that. Please check out the following FAQ on the possible implementations of that.
[FAQ…
Hi William,
Thank you for your reply.
I understand.
For driving SiC, LMG1210 is not suitable.
I'll introduce the UCC27301A-Q1 or the UCC27311A-Q1 that you recommended.
I appreciate your great help and cooperation.
Best regards,
Shinichi
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27301A-Q1 , UCC27311A-Q1 , TIDA-01407 , UCC27211A-Q1 , DRV8300-Q1 Hi Team,
I'd like to ask you about the high-side and low-side driver for 48V EV battery system. I couldn't find these devices…
Part Number: SM72295 Other Parts Discussed in Thread: UCC27301A-Q1 , UCC27289 , UCC27211A , UCC27201A , UCC27282 , UCC27284 , UCC27311A-Q1 , BQ2031
Is it possible to use this part in a single half-bridge configuration i.e. the 'A' side to implement…
Hi Vasu,
I apologize, but I just realized that the UCC27301A-Q1 I recommended has cross-conduction protection, so you would not be able to have both outputs enabled at the same time. The UCC27311A-Q1 has the same low-current specs without cross-conduction…
Part Number: UCC27301A-Q1 Other Parts Discussed in Thread: UCC27282-Q1
Tool/software:
Wireless charging for mobile devices in automobiles is a common and convenient feature. These chargers are typically powered from the 12V battery system but in some…
Other Parts Discussed in Thread: UCC25800 Most applications including power delivery for industrial and automotive utilizing a half-bridge gate driver use the bootstrap diode and boot capacitor to generate the high side driver bias. This is the simplest…
Part Number: UCC27301A
Tool/software:
Attached below is the .zip file for the PSpice project that contains a few different schematics that allow for testing the driver and its characteristics with respect to operating conditions set forth by the desired…