Part Number: UCC27423 Other Parts Discussed in Thread: LM5163 , LM317 Hi,
I am designing a RGB array control and I have a few questions.
The array is made up of a bunch of series and parallel LED strips. The power supply is a DC 40V power pack. The…
Part Number: UCC27423 Other Parts Discussed in Thread: UCC27524 , UCC27324 Hi Expert,
I have two questions about the MOSFET gate driver.
1. Drive with negative voltage with UCC27423
Is it possible to use UCC27423 for negative voltage drive application…
Part Number: UCC27423-Q1 Hi support team,
Questions concerning the UCC27423-Q1 datasheet(SGLS274H).
Values are different in "7.6 Switching Characteristics", "Figure 13", "Figure 14", but are figures correct?
For example, in Figures 13 and 14, Tr…
Part Number: UCC27424-EP Other Parts Discussed in Thread: UCC27423-EP , I am driving a gate drive transformer (240uH) with the UCC27423-EP, UCC27424-EP gate driver IC outputs. Do the integral body diodes of the MOSFET outputs protect the outputs of the…
Part Number: UCC27423 Other Parts Discussed in Thread: SN6501 , UCC27710 , UC3842 Hi Sir,
May I learn from you do we have any solution could replace IR25603 and has “Self-Oscillating”?
Thank you.
Edward Chen
Part Number: UCC27423-Q1 Hi TEXAS team,
Customer want to know the below parameter of UCC27423-Q1. Please help to provide. Thank you!
1. max value of Logic 1 input threshold;
2. min value of Logic 0 input threshold.
Kind regards,
Yingzhe X…
Other Parts Discussed in Thread: UCC27423 , UCC27423-EP I am simply trying to find out the recommended components to use on UCC27423 circuit. The circuit displayed on pg 1 simply shows an inductor, a p-channel MOSFET, as well as R1, C1 and Cout. Are there…
Other Parts Discussed in Thread: UCC27423-EP Please advise on what external components to use on UCC27423-EP for Figure 24: Typical Application Schematic. Desire Vout=5V @ Iout=4A. Thank you.
David
Part Number: TPS2814 Other Parts Discussed in Thread: UCC27423 , UCC27424 , UCC27444 , UCC27425 Tool/software: Hello Team,
Customer is looking for alternative for TPS2814DR. I have proposed UCC27424DR but customer thinks that the input and output logic…