Part Number: UCC27511 I am using UCC27511 single channel gate driver to drive 700W LED module (Output Voltage 375 to 390). We are implementing non inverting driver configuration as in application note (Fig 25 in datasheet) to drive mosfet PSM20N60CT.…
Part Number: UCC27511 Hi, I want use TI Mosfet Gate Driver UCC27511 for drive TWO PARALLEL MOSFET.
I have a doubt: 1) The connection of the two output (OUT_SRC / OUT_SNK) with resistor at the two Mosfets ??? may be correct the sink and source resistor…
Part Number: UCC27511 Hi Team,
Can UCC27511 operate at high frequency input? These parameters isn't related to input frequency?
1) tr, tf
2) Isrc, Isnk
Regards,
Kotaro Yamashita
Hi Maria,
Welcome to e2e! thanks for asking about UCC27511, Im an apps engineer supporting this device.
Whats your application? You mention an isolated gate driver. UCC27511 is not isolated, do you require an isolated gate driver?
Is the GND pin…
Part Number: UCC27511A-Q1 Other Parts Discussed in Thread: UCC27511 , I wish to model UCC27511A-Q1, but wasn't able to find a PSPICE model. However, I could find the UCC27511 model. They seem to very similar parts, and I was wondering if the models are…
Part Number: UCC27511 Other Parts Discussed in Thread: UCC27512 Hello team,
I noticed the UCC27511 datasheet abs max rating table, the OUTH has only indicate DC is -0.3V but no pulse spec, and OUTL has -2V for pulse spec, can you tell why?
When if…
Part Number: UCC27511 hai,
i am in the process of designing a new inverter. I placed three mosfets in parallel across the upper end of the transformer and and want to drive the three with a single gate signal.
i would like to use mosfet driver ucc27511…
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27511 ,
Switch-Mode Power Supplies and Merchant DC-DC converter applications often require high current drive and hard switching to drive large loads. This hard switching of the power switches…