Part Number: UCC27511A Other Parts Discussed in Thread: UCC27301A Tool/software: Hi Team,
Want to know if the device can be used similar to Infineon 1EDNx550 when used as high-side driver. Can I used as same way as the circled area in the pic below…
Part Number: UCC27511A Tool/software: May I know we have differential input solution to replace 1EDN7550? I had suggested UCC27511A, but it's not compatible with 1EDN7550.
1EDN7550, https://www.infineon.com/part/1EDN7550B
BR,
Gary
Part Number: UCC27511A Tool/software: Hi All,
I have a question about how to select R1 and R2, which are listed on the datasheet. I would like to drive an N-ch FET with as little delay as possible. In that case, should both R1 and R2 be set to 0 Ω?…
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27531 , UCC57108 , UCC57102 Tool/software: Hi team,
I am writing to check do you have a higher UVLO version (like 8.0V) that is p2p with UCC27511A? If not, do you have recommended part that…
Part Number: UCC27511A Hi TI,
I built a half-bridge buck converter as shown below using EPC2031 switch and UCC27511A as driver for both high side and low side switches.
For the low side gate driver the ground node is connected to the power ground…
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27511 , UCC27531 , , UCC27624 , UCC27614 Tool/software: HI
I am Driving two parallel mosfets for PFC using one driver IC ucc27511
or else I can use dual channel driver ucc27531 for two MOSFETs…
Part Number: UCC27511A-Q1 I require the lib file for
UCC27511A-Q1 as i need to model the gate driver in SABER, if any gate driver resembling this part , you can also share.
Part Number: UCC27511A-Q1 The driver UCC27511AQ was damaged whenever the PFC voltage of 390V builts up (whenever IC comes into action which is above 65V output ) Mainly PIN 1 (VDD) and PIN 2((out1) tracks were damaging. Is there anything to do with the…
Part Number: UCC27511A Hi,
Good Day. I have a customer who is working with UCC27511A. Please see below his query for you reference. Thank you very much.
It would be possible to keep the OUTH pin of UCC27511A in high state indefinitely?
I am driving…