Part Number: UCC27511A Hello!
Can you make a statement about the capacitance on the inputs of UCC27511A ?
It seems not to be part of the datasheet. However, my customer wants to add an r-c filter to adjust interlock time. Ideal would be data over temperature…
Part Number: UCC27511A Hi team,
A customer is looking for a gate driver for an 80W HF application at about 40MHz. So they are looking for a small bandwidth, high power gate driver. Can you recommend a part?
Thank you,
Franz
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27525 Good morning,
I would like to connect the +IN input of a UCC27511A low side driver to the -IN input of another UCC27511A.
Is it possible without the drivers influencing each other?
The one…
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27531 , Dears, I am looking for an alternate part to replace the UCC27531 .
Do you think that the UCC27511A can work? What makes the UCC27531 rated for SIC, is there any other difference exept of…
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27511 ,
Switch-Mode Power Supplies and Merchant DC-DC converter applications often require high current drive and hard switching to drive large loads. This hard switching of the power switches…
Other Parts Discussed in Thread: UCC27511A Customer is using UCC27511A, but they want to have Voff= 8V. Do you have any suggestion or any other suitable device? Thank you.
Part Number: UCC27714 Other Parts Discussed in Thread: UCC27511A-Q1 , UCC21551-Q1 , UCC27624-Q1 Tool/software: I am searching for a half-bridge device similar to the UCC27714 without interlock feature but it should be AEC-Q automotive qualified . As two switch…
Part Number: UCC27511A-Q1 Customers are considering using UCC27511A-Q1. In the data sheet, Ro(H) and RO(L) do not contain Min values. They want the Min value of Ro (H) and RO (L) in order to keep the drive current of the FET within the absolute maximum…