Part Number: UCC27511A-Q1 The driver UCC27511AQ was damaged whenever the PFC voltage of 390V builts up (whenever IC comes into action which is above 65V output ) Mainly PIN 1 (VDD) and PIN 2((out1) tracks were damaging. Is there anything to do with the…
Part Number: UCC27511A-Q1 I require the lib file for
UCC27511A-Q1 as i need to model the gate driver in SABER, if any gate driver resembling this part , you can also share.
Part Number: UCC27511A-Q1 Other Parts Discussed in Thread: UCC5350-Q1 Hello,
I have to design the High Voltage (800V) Heater System using Low-Side Switch circuit with IGBT
This system is similar to PTC Heater for HVAC.
https://www.rohm.com/documents/11303…
Part Number: UCC27714 Other Parts Discussed in Thread: UCC27511A-Q1 , UCC21551-Q1 , UCC27624-Q1 Tool/software: I am searching for a half-bridge device similar to the UCC27714 without interlock feature but it should be AEC-Q automotive qualified . As two switch…
Part Number: UCC27511A-Q1 Other Parts Discussed in Thread: UCC27511 , I wish to model UCC27511A-Q1, but wasn't able to find a PSPICE model. However, I could find the UCC27511 model. They seem to very similar parts, and I was wondering if the models are…
Part Number: UCC27511A-Q1 Customers are considering using UCC27511A-Q1. In the data sheet, Ro(H) and RO(L) do not contain Min values. They want the Min value of Ro (H) and RO (L) in order to keep the drive current of the FET within the absolute maximum…
Part Number: UCC27524A-Q1 Other Parts Discussed in Thread: LMG1020 , UCC27511A Hello ,
Need one support on finalizing dual output low side gate driver .
We are considering UCC27524A-Q1 for our application but we need very low operating current during static…
hello
I have a question about UCC27511-Q1
1,How many is the minimum pulse width? 2,How many is the maximum pulse width? 3,Is it subject to restrictions of a duty?
Thank you.
Part Number: BQ76920 Other Parts Discussed in Thread: UCC27511A-Q1 , , UCC27511A , UCC27511 , BQ77905
I want to drive 10 N Channel fets on both the Charge and Discharge side. IRLB3813 that require 57nC of gate charge each.
Can the drivers in the BQ76920…
Part Number: LM5114 Other Parts Discussed in Thread: UCC27511A , UCC27511 Hello guys,
One of my customers is planning to replace UCC27511A with LM5114. At this moment, they have the following questions. Could you please give me your reply for them?
Q1.…