Part Number: UCC27517 Hello,
I am using the UCC27517 in PFC application.
The IGBT is blowing up at power up, when the PFC controller starts.
After investigation I found that I didnt connect pin 2 of UCC27517 to the PFC controller GND, but it is…
Part Number: UCC27517 Other Parts Discussed in Thread: LM5155 , Tool/software: Hi team,
Is it able to provide the input capacitance between IN+ and IN- pin?
This is needed to check the system work because the input is LM5155 (boost controller) and…
Part Number: UCC27517 Other Parts Discussed in Thread: UCC27714 Are there any driver ics for dual-tube forward power supply solutions?
Input voltage range: 175V-265V without PFC, output: 24V/10A
Part Number: UCC27517 Tool/software: Hello, I am using UCC27517DBVR in a low side configuration to drive 6 NMOSFETs (AOTL66912) used as a switch for a Battery Protection board. Requesting the team to verify if the schematic is okay. DSG_CTRL is connected…
Part Number: UCC27517 Other Parts Discussed in Thread: TIDA-010015 , Hello Sir/Ma'am,
I want to simulate the schematics of TIDA-010015(480W SMPS) design in SIMetrix software. But for this I have to use the SIMPLIS model of UCC27517. But unfortunately…
Part Number: UCC27517 Hi team,
Customer is skeptical of justification that PSPICE of this device, because the output structure is diffrent with Figure23 in datasheet.
Datasheet is Pch / Nch parallel opeation however, PSPICE model is only driven by…
Part Number: UCC27517
Hi Team
There is a good new that we DIN UCC27517 !
Please help confirm the SCH is ok? THX
Spec : Vin=90~264Vac / Vo=54V / Io=15A
6864.CHARGERD3.pdf
Part Number: UCC27517 Hi Team,
My customer wants to know should they connect output of UCC27517 together or not when driving 2 MOSFET by 2 UCC27517,
could you kindly help confirm it and let me know the reason of your answer? Thanks.
Please let me…