Part Number: PMP8740 Other Parts Discussed in Thread: UCC28180 , , UCC28070 If I want extend the design to 2.5kw
for PFC boost stage & AUX what should I do
Part Number: UCC27517 Other Parts Discussed in Thread: SN74LVC1G14
In the screenshot the IN- pin is connected to Gnd. Is it required to route the In- parallel to the IN+ input. The operating speed is 5 MHz.
OUT signal is connected to the Cathode…
Part Number: UCC27517 Other Parts Discussed in Thread: UCC27714 , UCC27516
Hello forum gurus,
How can output sink 300mA continuous absolute maximum but also accept 500mA reverse, AKA negative current flow (Pg16,Fig.23)while the input is at CMOS low…
Part Number: UCC27517 Hello team,
Could you please let me know if IN pins accept 3.3V signal while VDD is off?
The datasheet mentions that Input Pin Absolute Maximum Voltage Levels Not Restricted by VDD Pin Bias Supply Voltage, but I'd like to make…
Part Number: UCC23511 Other Parts Discussed in Thread: UCC27531 , , UCC27517 Hi team,
Currently my customer is using the UCC23511, UCC27517, UCC27531 now. We want to check the pull up NMOS information. Whether the resistors below are typical?UCC23511…
Part Number: UCC27517 Dear Specialists,
My customer is considering UCC27517DBVT and has questions.
I would be grateful if you could advise.
---
Thermal information, Could you please let me know
(1)detail of evaluation board of si-taJA and si…
Part Number: UCC27517 Other Parts Discussed in Thread: STRIKE Hi
There is no LatchUp data on the datasheet. Do you have the data?
Regards,
Koji Hamamoto
Part Number: UCC27517 Hi team,
Could you give me advise if VDD (e.g. 12V) with pull up occurs on IN- pin or not? For example, can low voltage logic buffer (e.g. 3.3V) be connected to the IN-pin with VDD=12V?
Best regards,
Takeshi Sasaki