Part Number: BQ76200 Other Parts Discussed in Thread: UCC27517A-Q1 , UCC27517A Hi,
Currently, we are using the BQ76200 driving the separate Discharge, Charge and Pre-discharge FETs for High Side Switch path in a 54V EV BMS application;
- please…
Why should I replace 3-phase bridge drivers with half-bridge drivers in automotive AC compressor modules?
High-voltage 3-phase BLDC motors are used to drive the AC compressor in high-voltage HEV/EV. HVAC compressors, which can require 10 kW of power,…
Hi Shikha,
There are PSpice and TINA-TI models available in the CSD17382F4 product folder on the TI website. Click on the Design and Development tab and you should find them there. Please note, we do not publish unencrypted models on public websites.…
Hi Sundar,
Please see the following attachments.
The first excel sheet is the bom for the formatter board.
2514134E_dlpc120_formatter_BOM (1).xlsx
The second excel sheet is the bom for the dmd interface board.
2514105C_BOM.xlsx
Thanks,
Alex Chan
Yeah, you can look here:
http://www.ti.com/lsds/ti/amplifiers-linear/high-speed-amplifier-greater-than-equal-50MHz-products.page
It should be possible to find one that is pin-compatible too, but it is probably better to use a digital driver like the below…