Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: UCC27519 Other Parts Discussed in Thread: UCC21331 Tool/software: Hello, I would like to speak on teams if possible to learn which SiC gate driver IC is the best choice for me.
Thanks,
Chris
Part Number: UCC27519 Other Parts Discussed in Thread: UCC27517 I am trying to simulate the UCC27519 gate driver on PSpice for TI. Although I haven't changed anything on the schematic, I am not getting the expected results. The output is always 0V. The…
Part Number: UCC27519 Other Parts Discussed in Thread: UCC27518 Dear TI experts, The following is the circuit on our new product, please help to review whether there is any problem with the design, thank you!
Part Number: UCC27518 Other Parts Discussed in Thread: UCC27519
Team,
Note: it is known that the IN pin is CMOS level and the EN pin TTL level
-In order to use UCC27518 as alternative to UCC27519: Can the enable pin be used as a non-inverting input and…
Part Number: TIDA-01415 Other Parts Discussed in Thread: LM3409 , , UCC27519 Tool/software:
Hello, I had some questions regarding the TIDA-01415 design that uses the LM3409 as a LED driver. I’m attaching screenshots to help clarify the questions:…
CBT switches are designed for TTL signals, which do not actually go near 5 V. The switches are implemented with plain N-channel MOSFETs with the gate at 5 V, so with the signal at 5 V, the transistor is off.
There are proper analog switches using tranmission…
Part Number: UCC27519A-Q1 Other Parts Discussed in Thread: LMG1020 , UCC27611 Hi.
Quick question on UCC27519A-Q1 - what would be the maximum peak current when the device is supplied with 5V vdd ?
Thanks,
Part Number: UCC27519 Other Parts Discussed in Thread: UCC27517 , UCC27511A Hi
Can you help, we are using UCC27519, when VDD = 5V and IN+ is 3V square wave the device work correctly.
However when increase the VDD to 5.5V, In+ the same is 3V, there is no…
Part Number: UCC27519
Hi UCC27519 team,
could you please provide information on the max allowed power dissipation of the device?
There only seems to be a equation in the datasheet but no abs max specificaion.
Thanks,
Other Parts Discussed in Thread: UCC27519 I am currently working on a design using the UCC27519.
Datasheet lists the EN pull-up as 200k, IN+ pull-down as 230k.
Spice model for this part has EN pull-up as 200k, IN+ pull-down as 200k.
Measurements on real…