Part Number: UCC27524 Hi Team,
Need your help to provide component baking info for MPN “UCC27524DSDR” with MSL value “2” & Max thickness “0.8”.
Our internal team said that they are worried on the baking temperature 40 degree Celsius will melt the…
Part Number: UCC27524 Other Parts Discussed in Thread: UCC27624 , UCC27614 Hi expert,
If UCC27524 only uses one channel, can INA and INB be used in parallel? What parameters should be paid attention to during design? Thanks.
Part Number: TMS3705 Other Parts Discussed in Thread: UCC27424 , UCC27524A , Hello,
I use the TMS3705FDRQ1 together with UCC27524A, within the referencedesign described in manual SCBA021 "TMS3705 Range Extender Power Solution Using UCC27424"
I tried…
Part Number: UCC27524 Hi All,
I'm working on a design with this part and I was wondering if there was a recommended pcb land pattern for the DSD WSON 8 package. The documentation found on TI's website is only the physical dimensions.
Thanks!
Part Number: UCC27524 Hi Team,
My customer uses UCC27524 without any top side heat sink, is it applicable to estimate the junction temperature simply by Tcase + Power Loss(W)* ΨJT ?
In my customer's case, the power dissipation from IC itself is quite…
Part Number: UCC27524 Other Parts Discussed in Thread: UCC27624 Hi team,
My customer uses UCC27524 in their project. The customer has found that when doing a low temperature test (temperature below -20°C), the output of UCC27524 is sometimes pulled…
Part Number: UCC27524 Dear team,
Please help check the Input signal high threshold voltage at full temp range -40C to 125C for UCC27524DSDR.
We would like to know if it will have output when the PWM voltage is up to 1.8V.
Thank you!
Part Number: UCC27524 Hi team
We notice that EN is pulled up with 200kohm to VDD, if EN is connected to MCU with no pull-down resistor, will EN have VDD at IO pin?