Part Number: UCC27524 Other Parts Discussed in Thread: UCC27624 , The enable pins on this part have a nominal pullup of 200k ohms, along with an internal buffer. To do a worst case analysis disabling this part I need to know how much current will flow…
Part Number: UCC27524 I'm currently simulating a circuit using IN Multisim and I'm having trouble importing a UCC27524 SPICE model.
UCC27524.LIB
I am looking forward to getting the answer.
Thank you
Part Number: UCC27524 Other Parts Discussed in Thread: UCC27614 , UCC27624 Hello,
I am using the UCC27524 and I am experiencing several failures... I am not exceeding any of the datasheet specifications on the inputs or outputs...
The failure mode…
Part Number: UCC27524 Other Parts Discussed in Thread: TPL7407L , UCC27424
Hi
I was planning to use UCC27524 for Driving FO Transmitter @ 100 kHz
For the reqd distance, I was planning to pump some 70 mA thru' HFBR1521Z.
I would like to know the…
Part Number: UCC27524 When I apply power to the chip it draws more than 50 ma. I have no load, and the chip gets hot. This happened on the first 2 chips. The marking on the chip is a 6BAHJDM E4 27524, and it has a TI logo. Is this a UCC27524? The IDD…
Part Number: UCC27524 Other Parts Discussed in Thread: BQ76940 , Hello
I am designing a BMS using the BQ76940, the required current rating is of 250A therefore I am using parallel MOSFETs for Charge and Discharge control. Due to the limitations of BQ76940…
Part Number: UCC27524 Dear Team,
Could you help to check the schematic as below?
it's a inverter application.
Spec:
Vin 12V Vout :54V ac 60W
Many Thanks,
Jimmy