Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27624 , UCC27531 Tool/software: I am planning to use the UCC27531-Q1 2.5-A and 5-A, 35V MAX VDD FET and IGBT Single-Gate Driver to drive the SCT2H12NZ 1700V, 3.7A, THD, Silicon-Carbide (SiC…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27531
Tool/software:
Hi,
If the UCC27531 is operated at voltages exceeding the V(gs) maximum rating of an external MOSFET (typically 20 volts), the gate drive voltage will have to be limited…
Part Number: UCC27531-Q1 Hello,
is it possible to directly connect OUTH and OUTL and route this lane to one single gate resistor?
Like in the modified picture below:
Thanks and best regards,
Michael
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27301A-Q1 , UCC27311A-Q1 , TIDA-01407 , UCC27211A-Q1 , DRV8300-Q1 Hi Team,
I'd like to ask you about the high-side and low-side driver for 48V EV battery system. I couldn't find these devices on…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27624 , UCC27531 , UCC5350 , UCC5350-Q1
Hi, I'm having some troubles with the UCC27531QDBVRQ1.
In case of a pulse width with less than 30ns the gate driver is being short-circuited.
After an…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27614 , UCC23513 , UCC27532-Q1 , UCC27624-Q1 Hi,
I am looking to drive the SiC Mosfet requiring -5V and 18V Vgs.
Also the sink current is 2.81A and source current is 2.56.
If I am not wrong,…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27531 , TDC1000 I am currently powering VDD at 30V and everything works well, input max is 5v
I want to look for a new IC which has similar function/footprint as this UCC27531 but has higher voltage…
Part Number: UCC27531-Q1 Hi,
I am Using Gate Driver UCC27531-Q1 to drive MOSFET PMV50XNEA (as a switch).
The circuit as shown below.
Input will be driven by controller.
Source - D5V0
Gate - Output of Gate Driver
Drain - Output (5V or 0V based on controller…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27531 , UCC27532 UCC2753x series datasheets specify turn-on and turn-off propagation delays over -40 to +140°C temperature range. However, it isn't immediately clear whether these are typical…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27531 Hi, Team,
UCC27531/2-Q1 have separated outputs(OUTH & OUTL).
Can we connect the FET gate with both OUTL and OUTH pins shorted? Are there any concerns such as through current?
Regards…