Part Number: UCC27532-Q1 Dear expert, We will be using the UCC27532-Q1 IC for our project but we need below parameters:
Failure Mode Distribution
Pin FMEA
Can you provide parameters above?
Your help would be appreciated. Best regards,…
Part Number: UCC27532-Q1 Hello, My customer is asking me if the device is damaged when the output pin is short to GND. Does this device have any protection for output to GND short case?
Regards, Oba
Part Number: UCC27532-Q1 Hello
It is said that the UCC2753x can be used in parallel. How is it guaranteed that all the devices switch to the same time and there is no shoot-through because a high side switch of one device it on to the same time as a…
Part Number: UCC27532-Q1 Other Parts Discussed in Thread: UCC27532 , UCC27531-Q1 , UCC21520 Hi Team,
I want to drive SiC FETs. De to the typical high capacitance and high drive voltage (15-20V), I want to put 2 x UCC27532 in parallel. Will that concept…
Part Number: BQ24703 Other Parts Discussed in Thread: UCC27532-Q1 Hello
If the PWM signal is output higher than VCC like the waveform below, is there any possibility of damage?
Can I add a resistor to the PWM signal to protect against PMW transients…
Part Number: BQ24703 Other Parts Discussed in Thread: UCC27532-Q1 Hello
I want to insert a resistor into R80 to reduce the oscillation of the PWM signal.
How range can the R80 resistor value?
Is there any other way to reduce the oscillation of PWM…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27614 , UCC23513 , UCC27532-Q1 , UCC27624-Q1 Hi,
I am looking to drive the SiC Mosfet requiring -5V and 18V Vgs.
Also the sink current is 2.81A and source current is 2.56.
If I am…
Hello Tateo,
I do not see any issue with this application. One of the things to see is; the source current of UCC28730 is 35mA and the driver only requires 300uA to startup.
I would like to point out that the VDD max for UCC28730 is 38V however for…
Part Number: LMG1020-Q1 Other Parts Discussed in Thread: LMG1020 , UCC27532 , UCC27517A Dears,
I need technical insight for the following issue.
I have the requirement of Gate pulsing of an RF GaN FET and pulsing requirements are as below,
The device…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27531 , UCC27532 UCC2753x series datasheets specify turn-on and turn-off propagation delays over -40 to +140°C temperature range. However, it isn't immediately clear whether these are typical…