Hello Chang,
The UCC27710 driver turn on current is determined by the internal driver pull up device characteristics and internal driver pre drive voltage to the driver internal device in the output stage. If the external gate resistance is low enough…
Part Number: UCC27710 Hi, what is the internal pull-down resistance on the input pins for this device? I just see on the datasheet this spec for output pins, but not for the input.
Part Number: UCC27710 Hi team,
Does UCC27710 have any power sequence, timing, any dv/dt requirement to turn on and off for VDD and VHB?
Best regards,
Takeshi Sasaki
Part Number: UCC27710 Hi team,
Does this device have any package information on the insulation specification like creepage, clearance, isolation voltage?
Best regards,
Takeshi Sasaki
Part Number: UCC27710 Hi team,
Does UCC27710 have any dv/dt requirement on input pins (HI, LI)? I assume pull-down resister on the input pins and hysteresis input prevents from issues caused by dv/dt like https://www.ti.com/lit/an/scba004e/scba004e.pd…
Part Number: UCC27710 Other Parts Discussed in Thread: UCC27282 Dear Sir,
Currently using UCC27710 - 3No's to drive 6 Mosfets Please suggest 6 Channel version of UCC27710 to 6 No's Mosfets bridge inverter.
Regards Murthy
Part Number: UCC27710 Hello
I have a question for UCC27710.
The datasheet specifies absolute max value of “Output current, I OUT_PULSED(300ns)” as “1.0/-0.5A”.
Does the user have to check and make sure that the peak sink/source…
Part Number: UCC27710 Other Parts Discussed in Thread: TIDA-01606 , TIDM-02008 , PMP40690 , TIDA-010210 , TIDM-1007 Hello,
Please note that the following question has been posed for 4 weeks now without any useful answer. Please also note that we have asked…
Part Number: UCC27710 Hi Team,
My customer is using UCC27710 in UPS application, is it necessary to remove the PCB between Pin 5 (LO) & pin 6 (HS) to ensure creepage distance?
thanks a lot.
Best regards,
Yang
Part Number: UCC27710
Hi team,
The customer finds a issue that the high-side driver and low-side driver of UCC27710 could conduct at the same time, resulting in broken down. This failure happens and is reproducible it is powered up and powered down for…