Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712 , UCC27714 Tool/software: Hi,
UCC27712 claims 700 maximum voltage. When both high side and low side gate drivers are working, the voltage on pin 6 (HS) is high voltage (e.g. 200 VDC) and…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27211A-Q1 , UCC27712 , LM5109B-Q1 , UCC27311A-Q1 , UCC27301A-Q1 Tool/software: UCC27712-Q1 is this of ASIL B compliance? If not can you suggest any ASIL B half bridge for a 48 V system
Part Number: UCC27712-Q1 Tool/software: I am referring application note SLUA887A. in the page no 6 below attached waveform is given for Rboot = 0 ohm. in the details it was mentioned like Ch4 (green color) is VDD,
1) is fast ramp VDD is applying externally…
Hi Kobayashi-san,
As it's been almost a month without response, I will be closing this thread. Feel free to reply to reopen if you question still needs attention.
Thanks, Rubas
Part Number: UCC27712 Other Parts Discussed in Thread: UCC21551 , UCC21331 , UCC21231 Tool/software: is UCC27712 a isolated HVIC? I want to use it to drive 3 phase motor or two phase step motor
1,for step motor
a) under what voltage, for example, 100V…
Part Number: UCC27712 Tool/software: Hello,
Can i know the process technology/Wafer technology of the above mentioned Part number(UCC27712QDRQ1)for our critical aerospace applications, our client required to provide these data . thank you
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: ISO5852S , UCC27712 Tool/software: in the UCC27712-Q1 datasheet mentions below diagram for propagation delays measurement. for example tPDHL is measured from PWM 50% to HO 90%. similarly tPDLH is…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712
Tool/software:
Hello CC,
We are using UCC27712-Q1 in one of the BMS application. Where this part is used as a charge pump.
When charge pump starts working and Main BDU Mosfet ON (with…
Part Number: UCC27712-Q1 Tool/software: Dear support,
We have used 2 Nos UCC27712-Q1 devices' as attached schematics.
Here we have made a charge pump using UCC27712-Q1. A boost voltage from the charge pump is being used to drive mosfets (4+4) with…
Part Number: UCC27712 Tool/software: Hi,
I am trying to implement a circuit using the UCC27712 based off of the PMP23338B reference design.
In the attached scope shot
Yellow -- HO referenced to HS (ignore voltage scale)
green -- LO
Blue -- HI
Red --…