Part Number: UCC2800-EP Other Parts Discussed in Thread: UCC2800 Hi,
We intend to use UCC2800 just for its internal overcurrent detection feature. Now, we understand that for this feature to work the design has to ensure that the voltage at CS pin has…
Part Number: UCC2800 Hello. I see the CS pin has a range of 0.9V to 1.1V range for current limiting operation, but this amounts to a large range of load current in the end product. Am I missing something? If not, is there a tighter tolerance chip that…
Part Number: UCC2800 Other Parts Discussed in Thread: UCC2818 , Hello,
The initial tolerance of the oscillator, does it include the resistor and capacitor tolerance? If so what were the tolerance of the R & C to get the data sheet numbers? You got to have…
Part Number: UCC2800-Q1 Other Parts Discussed in Thread: UCC2800 , UC3842A , UC3842 Hi HVC team,
Question above. The max duty cycle is 100%, is it possible to limit to 80% (for example)?
Thanks, Lauren
Part Number: UCC2800-EP Other Parts Discussed in Thread: UCC2800 Hi team,
I've been noted that the UCC2800 frequency range is noted in the datasheet as 46KHz Typ. But the device is rated up to 1MHz.
Is this a typo or the greater frequencies requi…
Part Number: UCC2800 Other Parts Discussed in Thread: UC3842 , UCC2803 Question regarding application of UCC2800 series:
1) Can I use it in a boost application? I do not see any conflict , given that its max D is almost 100% & control is the same scheme…
Part Number: UCC2800 Other Parts Discussed in Thread: UCC28089 , Hello team.
I would like to have an application to achieve sync_operation with UCC2800 by using UCC28089 SYNC signal.
Now we are examining an attached configuration to do it.
- If you have anything…
Part Number: UCC2800-EP Colleagues, I have recently required clarification on thermal analysis for the UCC2800-EP package, so as to be able to predict operational conditions versus lifetime. This was posted here but there were no updates to the thread…