Hi Asha,
Asha C said: Gain in current sense section ,
UCC2801 gain varies from 1.1 to 1.8V. This is lower compared to the UCC28C43 gain which varies from 2.85V to 3.15V.
Because the internal gain is lower inside of the IC, this will affect the total…
Part Number: UCC2801-EP Other Parts Discussed in Thread: UCC2801 , UCC28C55 Hello,
I am using the UCC2801 on a flyback configuration in current mode to drive LEDs.
Vin = 300V to 400V
Vout = 60V
Freq=200KHz
The issue is that the component is…
Part Number: UCC2801-EP Other Parts Discussed in Thread: UC2845 , UCC2891 , UCC2801 hi, I have one question
I use UC2845 for 2switch forward converter
UC2845 doesn't have protection from short circuit, so I test UCC2891
Test
Insert UCC2891 instead…
Part Number: UCC2801 Hi Team, aside from the operating temperature are there other significant differences between the UCC2801 device?
Our customer is using this part on buck topology in current mode. And what they saw is that the DG4 has a current…
Hi Steven, Thank you for your reply. Here's the Rev D slus270d.pdf Kindly see below the snippets.. Furthermore, I've checked the SLUS270F, it seems that the "line regulation" for the UCC380x is not copied on SLUS270G. Can you please help confirm? Thank…