Part Number: UCC28019AEVM Other Parts Discussed in Thread: UCC28019A Tool/software: Hi
We would like to evaluate and speed up our design. Do you have the PCB (Altium Designer) files?
Part Number: UCC28019AEVM Other Parts Discussed in Thread: UCC28019A Hi,
I an designing a PFC boost using the UCC208019A.
Is it possible to receive the Gerber files or a pdf of the EVM board?
Also,
Is there a datasheet for L1?
Thanks,…
Part Number: UCC28019AEVM Other Parts Discussed in Thread: UCC28019 , UCC28019A We are re-designing an older line of products to meet PFC requirements where we have a low voltage PFC stage operating from a 36V step down transformer, with a required output…
Part Number: UCC28019AEVM Other Parts Discussed in Thread: UCC28019A Hello,
My customer tested the gave drive waveform on UCC28019A EVM and results are shown as below. The test condition is 110V input, 200W loading. They measured the waveform using…
Part Number: UCC28019A Other Parts Discussed in Thread: , UCC28180 , UCC28056 , UCC28019
Hi,
I am considering using UCC28019A for a PFC / boost converter in motor-drive application.
The target specifications are:
- Input: Rectified 100VAC…
Part Number: UCC28056 Other Parts Discussed in Thread: UCC28019A , UCC28180 , , UCC28019 , , PMP40580 , PMP22087 , UCC28019AEVM
Hi,
I previously posted the following question regarding a PFC / boost converter design using UCC28019A:
[Original…
Part Number: UCC28019 Other Parts Discussed in Thread: , UCC256302 , UCC256402 , PMP40379 , TPA3255 , , UCC28180 , UCC28056 , TIDA-010081 , UCC25640 Dear Sir/Ms.
May I request UCC28019AEVM schematic and layout source file include BOM for evaluation…
Hi Samuel,
Thanks for the update. I highly recommend getting a current probe as magnetic components are hard to debug without measuring current. If you do not have a current probe available, you can try measuring the voltage across your current resistor…
Part Number: UCC28019A Dear All,
For UCC28019AEVM 350-W PFC Converter. I have one issue.
What Type cap we can use for the "C4".
Original Circuit uses film Type .
Would we use ceramic type ?
If not , would you explain Why ?
Edward wu