Part Number: UCC28060 Other Parts Discussed in Thread: UCD3138A , Tool/software: Hi,
We are looking for a TI solution for 3-phase bridgeless PFC with high efficiency.
Our input voltage range shall be 20-24VAC, and output power requirement is 2.5KW…
Part Number: UCC28060 Hi team,
Does UCC28060 supporet AC 400Hz application?
Is any specific care about needed to design AC 400Hz PFC with UCC28060?
Best regards,
Kazuki Itoh
Part Number: UCC28060 In the SLU299A reference design document, the coils L1 and L2 are wound on Ferroxcube E41/17/12 cores. Is there a winding drawing available. Is it possible to buy the PR735 as an Eval board? What is the turns ratio between the main…
Part Number: UCC28060 Dear TI Team,
What will be the limitation to select Fmin.
In the datasheet application note 300W , Fmin selected as 45KHz. and Calculated Inductor Value =340uH.
1. Is it possible to increase Fmin to 100Khz and Calculate the…
Part Number: UCC28060 Dear TI team,
In the Datasheet of UCC28060
www.ti.com/.../slus767e.pdf
Inductor is calculated as per below formula
As per my understanding since the IC operates in Transition Mode , the formula should be
Please give…
Part Number: UCC28060 Hi all,
I made a design with the interleaf controller and everything is working very good except with a input around 115Vac.
The load on the PFC is around 600W when it happens.
If I put 115Vac on the input and I measure on…
Part Number: UCC28060 Other Parts Discussed in Thread: UCC28065 , UCC28064A Dear TI Team,
We are using the PFC IC UCC28060 (Transition Mode Two Phase Interleaved)
I am bit confused to select the optimized inductor for my application .
I did the…
Part Number: UCC28060 Hello.
What is the role of D3 in Figure 30 of the IC data sheet?
Some evaluation boards are not included depending on the design.