Part Number: UCC28063A Other Parts Discussed in Thread: UCC28070 My customer would like to know if it is possible to interleave four UCC28063A devices for a single output (from a single source)?
From some other posts it appears this will not work but…
Part Number: UCC28063A Good morning,
I am designing a 400W PFC with the UCC28063A.
My Vin range will be 184V RMS to 265V RMS.
To keep the inductor values small, I would like to use values of 114uH which will give a peak current of 7.58A at Vin = 184V…
Part Number: UCC28063A Other Parts Discussed in Thread: UCC28063 , LM5112 Hello all, What are some things to look for, to improve the phase relationship between Phase A and Phase B?
Right now I'm getting about a 100 ns error. The on-times are identical,…
Part Number: UCC28063A Other Parts Discussed in Thread: UCC28063 , UCC28810 , UCC28180 Hi team,
I have question about UCC28810 & UCC28063.
May I know UCC28063 & UCC28810 PF can cover VAC347~VAC530? Do you have schematic can share me?
Part Number: UCC28063A Customer want to use one chip UCC28063A for 720Wrms and 1.3kWpeak solution.
Is UCC28063A possible to use this solution?
If impossible, please let me know why impossible.
(I think that the reason is become very large external components…
Hello,Ray,
I may have confused the PMP10116 reference design with the SLUA625.
One used UCC28060 and one used UCC28063A.
UCC28060 ends soft start when Vcomp reaches ~ 6 V, UCC28063A when VSENSE reaches ~ 6 V.
What I want to know is how the slow start…
Other Parts Discussed in Thread: UCC28063A Hi there,
I'm designing a PFC module using UCC28063A and I'm having a few doubts.
If the output power drawn by the module I'm intending to connect to this PFC output decreases, what happens to the frequency…
Other Parts Discussed in Thread: UCC28063A Hi TI Team,
The output power is about 1000W and the output voltage is 750V. Is there a DCDC step-down chip recommended?
Other Parts Discussed in Thread: UCC28063A , UCC28180 , UC3854 , UC3842 Will the UCC28063A work for aircraft single and three phase power at 400 Hz. If not, what range of frequencies will it support?
Part Number: UCC28064A Other Parts Discussed in Thread: UCC28060 , UCC28063A , Hi Group,
SLUA625 details LED Driver Based on UCC28060 Interleaved ACDC Single Stage Flyback.
My application is low power (25W) but limits the transformer width to 19mm. Using…