Part Number: UCC28064A Other Parts Discussed in Thread: UCC28060 , UCC28063A , Hi Group,
SLUA625 details LED Driver Based on UCC28060 Interleaved ACDC Single Stage Flyback.
My application is low power (25W) but limits the transformer width to 19mm…
Tim
Section 8.3.9 (page 18) of the UCC28063 datasheet has details on soft start operation in UCC28063.
The way soft start works in UCC28063 is that there is a current source on the COMP pin that charges the capacitor. UCC28063 remains in soft start…
Part Number: UC2854B Other Parts Discussed in Thread: UCC28180 , UCC28056 , UCC28070A , UCC28063A , UCC28064A , UCC28065 Hi experts
I see that no behavioral models are available for the UC2854B.
Can someone recommend some similar newer devices with…
Part Number: PMP10116 Other Parts Discussed in Thread: UCC28063A , Hi team,
I have a customer that is testing reference design PMP10116, which uses UCC28063A. Unfortunately it isn’t working in a stable manner when the output voltage is adjusted.
Their…
Hi David:
there is no a pin special designed or showed PFC ok signal for downstream PWM controller, I would suggest you can add external circuit by sampling PFC bus voltage through Vsense pin and compare with a reference votlage with a comparator or…
Hi Rock,
UCC28064A can support interleaved flyback. We don't have a reference design with UCC28064A for interleaved flyback but we have reference designs of the previous gen UCC28063A for interleaved flyback: https://www.ti.com/tool/PMP10116
Best…
Hi Wei-Hao,
No model currently exists for UCC28061 unfortunately. A similar device, UCC28063A, has spice model available. UCC28063A is also an interleaved transition mode PFC controller. This device is also pin to pin compatible with UCC28061. Would…
Part Number: UCC28063 Other Parts Discussed in Thread: , UCC28061 , UCC28064A , UCC28065 , UCC28064 Can I get the unencrypted SPICE model for UCC28063 or any of the following IC:
UCC28061, UCCUCC28060, UCC28063a, UCC28063, UCC28064a, UCC28065.
Part Number: UCC28063 Other Parts Discussed in Thread: , UCC28061 , UCC28064A , UCC28065 , UCC28064 Hello,
Could you, please, provide unencrypted SPICE model for UCC28063 or any of the following IC:
UCC28061, UCCUCC28060, UCC28063a, UCC28063, UCC28064a…
Other Parts Discussed in Thread: UCC28019A , UCC28063A , UCC28064A , UCC28180 , UCC28070 We are looking for PFC controller that meet the following conditions.
Do you know the recommended IC?
Vin=90VAC~255VAC
Output=1.6kW 400V
CCM mode or Interleaved…