Part Number: UCC28064A In datasheet of UCC28064A, the calculation of the resistor connected between TSET pin and GND is somewhat blurry. Is there a more detailed documentation?
The fact we saw is that the component turns mosfet conduction at 2nd valley…
Part Number: UCC28064A Dear TI Support Team,
We are designing a PFC circuit using the UCC28064A control IC. The specifications are as follows:
PFC input voltage: AC 85 V to AC 265 V PFC output voltage: DC 400 V Peripheral circuitry around the control…
Part Number: UCC28064A Tool/software:
I need to know if the VCC input can be used for switching the system ON when power is already ON.? Currently we switch the AC input power on and off but would like to.leave that connected and just use the VCC. …
Part Number: UCC28064A Hi TI Team,
If caseA is used to feedback to VINAC, the power stage will be damaged. CaseB is normal operation. Why?
caseA(before bridge)
caseB(after bridge)
Part Number: UCC28064A Tool/software: Hi, TI
I have two questions. Please give me an advice.
1 As shown below, there are cases where it operates in single mode and interleaved mode depending on the input conditions. Is this normal? I'm particularly…
Part Number: UCC28064A Other Parts Discussed in Thread: UCC28064 , UCC28070 , UCC28180
Hello
We are looking for an interleaved PFC controller for 1500W PFC application.
We tried to design using the UCC28064, but the workbench indicated it's not…
Part Number: UCC28064A Hi team,
One of our customers is considering adopting a combination of the UCC28064ADR and UCC256614. They understand that the PFC on/off control can be managed via the TSET pin of the UCC256614. However, they are experiencing…
Part Number: UCC28064A Tool/software: Hello.
I am waiting for your reply.
Thanks.
========================================
Hello Yoon,
Thank you for bringing this matter to our attention.
I have notified internal management of these issues…
Part Number: UCC28064A Tool/software: Hello.
If you look at the datasheet of all semiconductor components, there are Absolute Maximum Rating and Recommended Operating Conditions.
Also, some companies kindly include the following phrases.
1. Functional…