Part Number: UCC2808A-1 Other Parts Discussed in Thread: UCC28083
Is UCC2808A or UCC28083 able to be configurated with open loop control? It means there is no feedback from output voltage, in stead it's used a fixed voltage supply to CTRL pin. if so…
Part Number: UCC2808A-1 Other Parts Discussed in Thread: UCC3808-1 , TL431 Hello,
I would appreciate if somebody could help me fixing a problem affecting an old design initially based on an UCC3808-1 and now using an UCC2808A-1.
Regards
Gilles …
Part Number: UCC2808A-1 Hi,
The datasheet lists IDD < 10mA with VDD at 15V.
However the sink current peak at VOUTA and VOUTB is 1A.
Isn't this current supplied by VDD?
If that is correct, is the average IDD < 10mA because those peaks are supplied…
Hi John:
UCC2808A-1 Can provide the correct output Voltage。Change duty cycle, this comp foot voltage does not change very much. meanwhile,Peak current is high at soft start。That's why?Is there a solution
Part Number: UCC2808A-1 Is it possible to achieve a circuit of Fig.2 of ucc2808 data seat? The input voltage area which is 72V from 36V by Push - Pull system, can it correspond?
Part Number: UCC2808A-1 Hi Team
for UCC2808A, calulating the proper sensing resistor is by { TYP overcurrent threshold[V] / OverCurrent[A] = 0.75V / OverCurrent[A] } ?
Other Parts Discussed in Thread: UCC2808A-1 I have quetions of UCC2808A-1.
1. stability
I think UCC2808A-1 is the voltage control by the width of ON time. Is this correct?
If it is correct, I think it is difficult to keep the stability of the wave…
Other Parts Discussed in Thread: UCC2808A-1 , TL431 Hi,
i will build a unregulated Push-Pull-Converter with the UCC2808A-1.
At fixed 200kHz it should run at nearly 90% Duty-Cycle.
The Current should be limited at nearly 1,2A.
I'm a little…
Part Number: UCC2808-1 Other Parts Discussed in Thread: UCC2808A-1 Tool/software: Hello,
I am an FAE at a distributor that handles TI products. My customer is considering an isolated DC-DC converter with the following specifications. My customer is…
Part Number: UCC28089 Other Parts Discussed in Thread: UCC2808A-1 Tool/software: Hi,
We are currently using the UCC28089 in our design. However, the datasheet only provides a high-level description of its usage, and we are looking for more detailed…