Part Number: UCC2808A-2Q1 Other Parts Discussed in Thread: LM25037 Hi,
Is there a SPICE model available for this device, or at least a similar device?
Regards,
B
Part Number: UCC2808A-2Q1 Hi,
What is the OUT Low Level and High Level voltage at VDD=5V? The datasheet shows the spec at VDD=10V, but I couldn't find the spec at 5V.
Best Regards, Taki
Part Number: UCC2808A-2Q1 Hi Team
I found my customer is using UCC2808A-2Q1 as below.
he don't use feedback due to board size limitation.
in this case, normally we connects FB to GND for Max Duty, and leaves COMP as floating.
however, he is…
Part Number: UCC2808A-2Q1 Is there defined absolute maximum rating for UCC2808A-2Q1 below?
・RC Pin: max voltage and current
・COMP Pin: max voltage and current
Best regards,
Satoshi
Part Number: LM25037 Other Parts Discussed in Thread: , UCC2808A-2 Tool/software: Hello Team,
I am looking for and DCDC controller for following application:
Input voltage: From Battery ~7V
Output voltage: Configurable to 250V and 420V
Output…
Riki,
I recommend using a Push Pull controller, which allows you to get high current capabilities at the primary side with a limited VIN value. Below, you can see the portfolio with for Push Pull controllers. As a personal recommendation, UCC2808A is…
Hi,
1. LM5045 does not have automotive graded parts. Also we do not have a part like LM5045 with automotive grade. We have two parts LM25037-Q1 and UCC2808A-1Q1, or UCC2808A-2Q1, but these need to have external bridge drivers to make full bridge converter…
Hi Josef,
Push Pull UCC2808A-1Q1 and UCC2808A-2Q1 can be used here.
https://www.ti.com/product/UCC2808A-1Q1
https://www.ti.com/product/UCC2808A-2Q1
Regards,
Teng