Part Number: TMS320F2800157-Q1 hi , Launchpad-F2800157 and DRV8323RS-EVM. With Universal Motor Control Lab. In Level 1 build。 hardware connected as blow.
set variable - motorVars_M1.flagEnableRunAndIdentify to 1 ,
According to the user guide, the actual…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH I tried building TI TDA4VH EVK SDK yocto build but got following error:
| ERROR: oe_runmake failed | WARNING: /home/k271k9/ti-processor-sdk-linux-j784s4-evm-08_06_01_02/yocto-build/build/arago…
Part Number: TDA4VH-Q1 Running Inference on Model - ../../../bev_patr1_tvm/bevdet_patr1_device
2024-03-29 21:37:39,150 INFO Could not find libdlr.so in model artifact. Using dlr from /usr/lib/python3.10/site-packages/dlr/libdlr.so
TIDL_RT_OVX: Set…
Part Number: TDA4AL-Q1 Hi TI,
front camera connect in csi0,surrond camera connect in csi1.
Now we have successfully swap CSI 0 and CSI 1.
How should we know if the current configuration is csi 0 or csi 1?
Why do we need to exchange captureObj ->params…
Part Number: DRV8889-Q1 Other Parts Discussed in Thread: DRV8899-Q1 Hi
How to connect to 1-2 phases stepper motor ? motor spec as below. thanks!
2_Q24BJ48-XXXXW_0_0-00WX-1(1).pdf
Part Number: TLV1805-Q1 The chip has no markings indicating pin 1, looks entirely different from the spec sheet. Marked only 1ULF with no other polarity indicator. WHICH IS PIN 1??
Part Number: LM5050-1-Q1 Hi do you have an FMEA for the LM5050-1-Q1? We are using the LM5050Q1MK-1/NOPB and need the pin failure modes for the device if it is available please.
Many thanks, Nigel.