Part Number: DS90UH947-Q1 Dear Specialists,
My customer is interested in FPD Link3 for Fiber cable transmission.
According to the related thread, without using backchannels, It is stated that it can be used if the specifications of the serializer and deserializer…
HI,
Diwakar Dhyani said: Are these hardware changes improving the recovery time ?
This has not been taken a lot of tests,but it is difficult to make completely determined conclusions.
Thanks
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM5143 , LM5143A-Q1 What are the difference between below 3 parts?
1. LM5143QRHARQ1 : top marking LM5143QR HARQ1
2. LM5143QRWGRQ1 : top marking LM5143A2
3. LM5143RHAR : top marking LM5143RHAR
Is there any…
Part Number: ADS1261-Q1 Hello,
I am looking for 3 wire and 4 wire RTD design using ADS1261-Q1. The datasheet provides only information on 3 wire circuit. Kindly guide us for 4 wire RTD design.
Part Number: LP87745-Q1 Hello,
we use the LP877451A1RXVRQ1 with a switching frequency of 17,6MHz set by OTP.
Is there any way to change the switching frequency to 8,8 MHz by software,
or we need a new OTP version?
Best Regards
Part Number: AM62A7-Q1 Dear expert,
Can we replace the C522 and C523 in the EVM with the common ceramic capacitor? And can we change the C522 from 10uF to 2.2uF? Thanks.
Best Regards,
Xingyu Zhu
Part Number: DP83TC814S-Q1 Hi
Please help suggest TI PHY solution to VIA . thanks.
1. A simple 1 to 2 hub
2. 3 ports switch hub (the host must support GBE TX/RX interface, not RGMII)
3. Application =>On our board, to output a set of GBE (TX/RX signal…
Part Number: BQ79606A-Q1 Hi team,
Interested application question for the BQ79606A-Q1. The BQ79606A-Q1 specifies a minimum of 3 cell voltage measurements.
Does it need to measure a minimum of 3 series-connected cells? or just three measurements?
In the…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5273 , When is this part scheduled for manufacture and when will it be available to order? We have a design that uses both the TMAG5273 and 5173 and will shortly be running a larger batch of…