Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com. when I click on the transformer, its showing popup with transformer information as CUSTOM…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com.
Another clarification required. you said NS1 is secondary and NS2 is auxillary. But the winding…
Part Number: UCC2813-5-Q1 Other Parts Discussed in Thread: TLV3501 Hi Team,
Our customer encountered an error when he imported the unencrypted PSpice model of UCC2813-5-Q1 to LTspice. The model is not working, showing too many nodes in the simulation as…
Part Number: UCC2813-5-Q1 Hi team,
Can you please check what is the thermal performance of UCC2813-5-Q1? The datasheet is too old it did not show any RθJA or RθJC, can you provide thermal information for UCC2813-5-Q1 in tabular format:
Many…
Part Number: UCC2813-5-Q1 Hi, I try to develop an isolated DC/DC with 9 - 32 V input and 12 V output with 3 A. If I decrease the input voltage under about 20 V, the output voltage is decreasing too. I think the problem is the current sensing of the controller…
Part Number: UCC2813-5-Q1 Other Parts Discussed in Thread: UCC2813-5 Hi team,
My customer wishes to know what is the REF OK threshold and hysteresis for UCC2813-5-Q1, the datasheet did not specify this value. Could you please help us to find it?
Thank…
Part Number: UCC2813-5-Q1 Hi
in datasheet, there is no this information, could you provide the Tj range of the Absolute Maximum Ratings and Tj range of Recommended Operating Conditions?
thanks.
UCC2813QDR-5Q1
Part Number: UCC2813-5-Q1 Hi there,
During testing it has been found that the switching frequency is half of what is expecting (expect 300KHz, have got 150KHz).
In document SGLS245D have got
Also, in SLUS161E we have found this note
Now I have 100pF…