Hello Edward,
Based on this rather limited set of requirements, the tentative answer is YES.
Can you please clarify if the input voltage Vin is AC or DC?
If it is DC, then yes the UCC28740 can readily support that spec since the HV input is rated…
Hello Alireza,
It is difficult to tell if that bobbin is designed to accept an EFD core just by looking at it. The shape of the bobbin appears to fit an EFD core shape, but only a datasheet for the bobbin will verify if its dimensions are correct for…
Yaita,
Here are some part numbers that appeared when I searched for your requirements. I recommend starting to look at UCC28600-Q1.
Part Number
TL2843B-Q1
UC2825A-Q1
UC2856-Q1
UC2856Q
UCC25706-Q1
UCC2813-0-Q1
UCC2813-1-Q1
UCC2813-2…
Other Parts Discussed in Thread: UCC2813-1 Hi,
I have designed Multi-output flyback power supply by using UCC2813-1 PWM IC,
Input and output specifications are as follows
Vinput- 16V-40V
Vout-5V@5A,+15V@0.75A,-15V@0.75A
Switching frequency -200kHz
The converter…
Other Parts Discussed in Thread: UCC2800 I am currently using UCC2800 for a 100 kHz 20, 5 output, flyback supply and a UCC2813 for a boost supply. I need to change the frequency to eliminate some EMI issues.
What controller part do you recommend for use…
Hello Emre,
Thank you for uncovering several typographical errors in the application section of our UCC2813-x datasheet. We will begin the process to correct these errors, but this may take many weeks due to internal procedures. Meanwhile, I’ll address…