Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC28019 , UCC28056 Hi,
Hope you are well. My question is whether the IAC pin of the UCC2818-EP has a specific voltage level, or if the level at that pin is zero. For example, is Riac sized by…
Part Number: UCC2818-EP Tool/software: Hi TI team,
We are planning to use UCC2818-EP in our design.
Following is our requirement
Vin :100Vrms to 134Vrms (360Hz to 800Hz)
Vout : 400V (24W)
As per datasheet, for the power level we have to use…
Part Number: UCC2818-EP Hi,
I want to confirm the maximum switching frequency of the UCC2818EP. Is it 120 kHz, or can it go higher? Thank you!
Kind regards,
Luis.
Part Number: UCC2818-EP Other Parts Discussed in Thread: UC2854B-EP , UC2854 , UCC2818 Tool/software: Hi TI team
I would like to know which among these PFC ICs (UCC2818-EP and UC2854-EP) can have <5%THD on the input current for input frequency of…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC28180 , PMP31164 , UCC25640EVM-020 Tool/software: Hi TI team
We have build a PFC board using UCC2818-EP PFC IC.
Following is our requirement
Vin :100Vrms to 134Vrms (360Hz to 800Hz) …
Part Number: UCC2818-EP Tool/software: Hello TI Team,
The reference design in the datasheet says that the capacitor across the Vref pin should be around 1uF. However, I was thinking of using a 4.7uF capacitor to make the pin more stable. Could you please…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC2818 , UC2854 Tool/software: Hi TI team,
I have following requirements
Input voltage -100Vrms to 134Vrms
Frequency- 360Hz to 800Hz
output voltage- 400V
output power 100W
I am…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC28070A Hello,
I will rectify the 3 Phase 400 Hz 115 VAC input supply to DC (270 VDC) with the bridge rectifiers shown in the figure, and then apply boost PFC to 450 VDC with the UCC2818-EP…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC3817 Hello team,
Does TI have any available EVM which is able to evaluate UCC2818-EP?
EVM for other p2p PFC is also acceptable.
Regards,
Itoh