Part Number: UCC28180 When dimensioning a PFC circuit based on UCC28180, we will use the excel tool from TI. When calculating the technical parameters of the PFC choke, the maximum peak current IL_PEAK is 17.5A and the boost inductor value LBST is 0.130mH…
Part Number: UCC28180 Other Parts Discussed in Thread: UCC28019A Hi
I have used UCC28180 IC for front end PFC operation at 1KW power EV charger
I am assigned to reduce to Power rating of 480W and 250W using same circuit.
Despite PFC not mandate for less…
Part Number: UCC28180 Hi
I am designing a 2.5KW PFC with ucc28180.
Vinmin=160
Vinmax= 270
Efficiency expected= 98
Vout= 400V
Based on a 40 percent ripple ( Inductor current) I calculated the boost inductor is 156uH.
I have the following questions
1) Whether…
Part Number: UCC28180 For a project with BLDC motor, we need a PFC circuit which has an input voltage range of approx. 90V...130V and a max. output voltage of approx. 150...200V (not yet finalised).The output power should be approx. 800W.
We have already…
Part Number: UCC28180 Other Parts Discussed in Thread: UCC27524 Hello Team,
We have designed the 1600W PFC design using the UCC28180. We are using the same chip for the different designs like 450W, 600W & 900W works well. But in the higher power 1750W…
Part Number: UCC28180 Hi Team,
I am not able to see pwm pulses at 8th pin of UC28180, I was applied 14.5Vcc at 7th pin.
Thanks and Regards,
Balakrishna
Part Number: UCC28180 Hi,
I am designing a 3phase pfc.I am planing to use single boost converter which is followed by a 3 phase rectifier(I know that getting 3phase sinewave is not possible and THD will be 32%,its ok for me). Please refer the image for…
Part Number: UCC28180 Hello,
Could you please advise how the chip will behave if the input is a Square wave DC, switching between 0V and 400V at 400Hz? I am wondering if this controller is going to limit the inrush current to the bulk cap at every switching…
Hello Conor,
I have not received any further reply to my last private email on Oct 24, 2023 regarding this issue, so I will close out this thread.
Regards, Ulrich
Part Number: UCC28180 Tool/software: We need to realize the power more than 120W PF value not less than 99%, power less than 120W PF not less than 90%, the maximum power of 250W, UCC281180DR this chip can be realized? According to the 350W circuit design…