Part Number: UCC28180EVM-573 Hi,
I need gerber file of UCC28180EVM-573 module for my pfc circuit design.
Kindly share the gerber file to my email ID sathishkumar@nashindia.com
Regards,
Sathish
Part Number: UCC28180EVM-573 Other Parts Discussed in Thread: UCC28070 Hi,
I have the following doubt;
1. While designing the PFC (Boost, CCM), the losses in the output bulk capacitor is Irms2*ESR.
Let us say, i am designing a 1200W PFC over the…
Part Number: UCC28180EVM-573 Other Parts Discussed in Thread: UCC28180 Hi, I am looking at the schematic of this UCC28180EVM-573. Noticed there is a diode D2 across the inductor and output diode D3. what is the purpose of this D2 diode? the datasheet…
Part Number: UCC28180EVM-573UCC28180EVM-573, I would like to know what would happen to the evaluation board with operating below its input voltage range with VCC turned-on. I would expect the board to go into over current protection mode, is this correct…
Part Number: UCC28180EVM-573 Other Parts Discussed in Thread: UCC28180 Hi, I`m currently using the UCC28180 EVM as a base for a 300W Boost PFC converter. (390Vdc)
We want to produce at least 250W at a lower than normal input voltage range.
We need…
Part Number: UCC28180 Hi ALL
Pls help me i need to know to improved output Voltage regulation of UCC28180EVM-573 with in 10% of output voltage .
The output voltage is drop about 52V .
Bestregard
Prarinya
Part Number: UCC28180EVM-573 Other Parts Discussed in Thread: UCC28180 , TIDA-00776 , UCC28019A , UCC28019 , TL431
Hello
We boguht the ucc28180evm-573 for evaluating the circuit.
But we ended with a problem, the evaluation module blown up at…
Part Number: UCC28180EVM-573 Customer is evaluating UCC28180EVM-573 for below condition, but when output power increased No load to 80W, FET was damaged.
Please let me know about possibility of the reason for FET break.
------------------------…