Part Number: UCC2818A-Q1 Hi team,
What is the maxium voltgae VFF pin can stand of UCC2818A-Q1, since i notice on datasheet, the VFF voltage only shows around 4.7V as below. Does this mean, the VFF voltage can not exceed 4.7V?
Best Regards,
Gene
Part Number: UCC2818A-Q1 Hi Team,
As I notice on datasheet figure 5, Typical Application Circuit, the Vline is 85-270Vac. From customer requirements, if Vline ranges from 70-280Vac, can the Vff go beyond 4.7V? Or in this case how could customer adjust…
Part Number: UCC2818A-Q1 Hi Team,
Customer calculate the loop parameter based on datasheet, , it works fine at Vin 85-270V. While at Vin=75V or below, with full load the loop is not stable. Is there any action customer could take to realize low line full…
Hi Someno-san,
If the synchronization is critical to the performance of the system then the synchronisation signal should be present when the UCC2818a starts up. If not then I think it ok to sync the UCC2818a after start-up.
Sorry I do not have a schematic…
Part Number: UCC2818A-Q1 Hi team,
At low line, customer found small current distortion while input voltage come across zero both on their board and our EVM, have you experienced with this phenomenon?
(Green is input current, yellow is input voltage,…
Part Number: UCC2818A-Q1 Other Parts Discussed in Thread: UC3854 Hi team,
My customers has questions on the UCC2818A-Q1 regarding the datasheet (see below).
Could you please help us to address them?
Thanks for your support.
Pol
---------------------…
Part Number: UCC2818A Hello.
I have a question.
We configured the power supply using UCC2818A. We are doing power supply operation test. UCC2818A stops when we perform the following operation test with the attached circuit. Why did it stop? It will not return…
Part Number: UCC2818A Other Parts Discussed in Thread: UCC2818 I designed a 3kw pfc converter . i sense current with 2 CT according to SLUA308 APP note.my fet is FCA35N60 (3 FET in parallel) and my diode is DSEI30-06A.my CT ratio is 260 to 1 and Rsense…
Part Number: UCC2818A-Q1 Other Parts Discussed in Thread: UCC28C43-Q1 Hello,
I am building an AC-DC converter with boost PFC which has an output voltage of 390V (1500W) using UCC2818A-Q1 IC. I am looking into the power supply options for this IC, I do…
Part Number: UCC2818A Hello.
We are considering UCC 2818A. I am thinking about designing the detailed part by carrying out the simulation to do the design. Could you give me the spice model of UCC 2818A? Thank you.