Part Number: UCC28220-Q1 Other Parts Discussed in Thread: UCC28220 Tool/software: Hello,
Can you please suggest the method how to calculate slope resistor for UCC28220 interleaved boost converter. The method given in datasheet is also wrong. Values calculated…
Part Number: UCC28220-Q1 Other Parts Discussed in Thread: UCC28220 Tool/software: Hi Team,
My customer wants to know the CDM ESD classification level of UCC28220QPWRQ1.
Could you help provide it?
Thanks,
Takashi
Part Number: UCC28220 Hi,
I am Arrshith. I am making a peak current mode controlled interleaved buck converter, So I am planning to synchronize two UCC280220 ICs with digitally generated multiphase pulses so that I get 4 PWM controller. is it possible…
Part Number: UCC28220
Hello,
I would like to know if this can be used to implement an interleave DC-DC buck converter, for example. I would like to know the steps from high voltage (800V) to low voltage (100V) without current at 60A.
I am trying to…
Part Number: UCC28220 Hi.
I am developing an interleaved 3 switch forward convertor using IC UCC28220 * T opology: 3 switch forward
* Input: 380VDC(PFC Output) * Ouput: 12VDC, 84A, 1000W The problem is the overcurrent protection circuit. The circuit…
Part Number: UCC28220 Other Parts Discussed in Thread: TL432 , TL431
Hi
On March 3rd, I inquired about the secondary side control of UCC28220 as follows and received a reply.
1. My inquiry: I want to know how to use UCC28220 for Secondary controlled PWM…
Part Number: UCC28220 HI
I designed an Interleaved 3 Switch Forward circuit using UCC28220. (3 Switch Forward circuit referred to TI patent data. See Attachment. File: 04 Overcoming the Duty Cycle Limits of the Two-Switch Forward - EE Times.pdf)
I designed…
Part Number: UCC28220 Other Parts Discussed in Thread: TL431 , TL432 HI
UCC28220.
I want to know how to use UCC28220 for Secondary controlled PWM IC. (UCC28220 must be designed on the secondary side and the feedback must be connected directly at output…
Part Number: UCC28220
We have some problems to clarify about IC ucc28220.
We use simplis to build ucc28220 model to simulate Interleaved boost converter. After the parameter adjustment for compensation, the Bandwidth simulation result can only be up…