Part Number: UCC28600 Hi Team,
I need support for my 200W output Flyback SMPS based on TI UCC28600 IC.
let me know how may i proceed for transformer design with multiple outputs i.e. 7 outputs.
ETD442215 my core selection, what is the switching…
Part Number: UCC28600 Other Parts Discussed in Thread: PMP10150 Hi all,
I have a question regarding Vdd voltage on UCC28600.
I saw a schematic in a reference design (PMP10150) the Vdd pin of UCC28600 is connected to a series of startup resistor from…
Part Number: UCC28600 Other Parts Discussed in Thread: UCC28056 During webench design, the UCC28600 design is obtained for the flyback 24V, 12A PWM controller. Nevertheless, the IOUT limit is shown as 10A on further Webench modifications. Please verify…
Part Number: UCC28600 Tool/software: Subject: UCC28600 – Observed Burst Switching Behavior Not Matching Datasheet
Question: Hello,
I am using the UCC28600 in my power supply design and I have observed a switching behavior that I would like clarification…
Part Number: UCC28600
Tool/software:
With UCC28600 IC, I got 1.2kHz bandwidth at full load and 100Hz bandwidth at average load but my switching frequency is of 40kHz , which component I should to tune to increase the Bandwidth of the system. where…
Part Number: UCC28600 Hello,
I'm designing a 30W Flyback converter using UCC28600 controller. I use the excel sheet SLVC104 provided by TI to calculate the circuit parameters.
As I understand from the datasheet, UCC28600 implements cycle by cycle…
Part Number: UCC28600 Other Parts Discussed in Thread: UCC27531 , UCC27532 , , UCC27537 , UCC57108 , UCC57102 Tool/software: Hi,
Which one be the best suitable gate driver UCC27531 or UCC27532 for sic mosfet, when my PWM controller is UCC28600 QR Flyback…
Part Number: UCC28600 Tool/software: Dear Team,
I am using the spreadsheet of UCC28600, and I found there is only one output provision, but I am designing 200W SMPS with 3 phase AC input for multiple output about 7 outputs.
So, what I need to do with…
Part Number: UCC28600 Tool/software: Hi Sir :
We encountered some issues while using TI's UCC28600. Please refer to our schematic diagram and the specific problems encountered below for assistance in analyzing. Thank you!
DC normal input: 380 * 1…
Part Number: UCC28600 I have a design that I am working on that has a ripple problem. At no load up to 0.2A the ripple is out of my spec, which is 150mV, my preference is less than 100mV. It's also a bit high at full load, but I'd rather focus on this…