Part Number: UCC28610 TI support,
I would like to start a new discsussion around our UCC28610 flyback power supply. I am not the original design engineer of this schematic. It has been in use for many years but we recently started having severe performance…
Part Number: UCC28610 Hi, TI
I used UCC28610 to configure the circuit with secondary feedback and output voltage is 12V as the attachment.
2. The output voltage is always about 5V when DRV output is a 20~ HZ flat sawtooth waves at the top, meanwhile…
Part Number: UCC28610 Tool/software:
Can the UCC28610 green mode flyback controller use all protections as latch-type protections? And is it possible to completely disable auto-recovery protection? For example, overload and overvoltage protections…
Part Number: UCC28610 Other Parts Discussed in Thread: UCC28742
Tool/software:
Hello,
I am designing a flyback converter based on the UCC28610.
Given parameters:
Minimum input voltage : 250V
Maximum input voltage : 800V
Maximum output…
Part Number: UCC28610 Hi,
I am using UCC28610DR, but I am having a hard time getting it. Please let me know if there is a similar product that can be replaced with P2P.
Thanks,
Astro
Part Number: UCC28610 Other Parts Discussed in Thread: UCC28600 , , UCC28780 , UCC28700 , UCC28730 , UCC28750 , LM5023 , UCC28781 Hi Team,
We are looking for a suitable IC for flyback control. Do you have an IC similar to the UCC28610 (valley switching…
Part Number: UCC28610
What are all the modifications required to use the above control circuit for 440VAC.
Mosfet, transformers will be selected according the rectified pk voltage.
Kindly suggest for thr required modification in the control circuit…
Part Number: UCC28610 Other Parts Discussed in Thread: TL431 Hi, TI expert.
The customer used UCC28610 to configure the circuit.
TL431 is applied to the secondary feedback stage and the output voltage is set to 15V, but it is said that the output…