Hello,
The UCC28911 for applications below 12 W so the design will work for either application. The device does not come in a Q1 rating. If you require Q1 rating for automotive the UCC28700-Q1 will work for this application and will require an external…
Hi Jaeyup,
Q1: 1st check the Vdd pin voltage of the UCC28700-Q1. It should be larger than 21V, less than 35V. Then check the PWM output at DRV pin, see if there is pulses coming out.
Q2: The problem is that you will not able to generate 600V output voltage…
Part Number: UCC28600-Q1 Other Parts Discussed in Thread: UCC28600 , TIDA-00386 , UCC28700 , UCC28630 Hello TI Power Management Gurus,
I want to design 150Vdc to +12Vd/5V output flyback converter with UCC28600. In the application 12V output, is not isolated…
Part Number: UCC28730-Q1 Other Parts Discussed in Thread: PMP10200 , UCC28700 According SLUA987B description,The UCC28730-Q1 can design Automotive 40V to 1kV input flyback converter,but Ivsl(run)=220uA,Ivs(max)=-1.2mA,The input voltage range maximum 1.2…
Part Number: UCC28730-Q1 Other Parts Discussed in Thread: TPS40210 , UCC28730 , LM25180 , UCC28910 , UCC28700 , UCC28911 Hello,
Can you confirm me if possible to use UCC28730 instead of TPS40210?
The price of TPS40210 is high and i need a driver with quasi…
Other Parts Discussed in Thread: UCC28C45-Q1 , UCC28C43-Q1 , UCC28700 , UCC28C45 , UCC28700-Q1 , UCC28C43 , UCC28730 Hello team
My customer is looking for flyback converter with following operational condition.
Input voltage : 30V - 450V DC
Output Voltage …
Kazuya
It is against TI policy to publicly comment on any potential future device.
If you need improved transient response, I recommend considering UCC28700-Q1. This is another Q100 rated flyback controller that does not need the wake-up IC to achieve…
Part Number: UCC28700 Other Parts Discussed in Thread: TINA-TI , Hi team,
My customer wants to change turn ratio of the transformer model in the "UCC28700-Q1 TINA-TI Transient Reference Design" (TX1 CUSTOM). I am not familier with SPICE macro…
Part Number: LM5141-Q1 Other Parts Discussed in Thread: PMP20345 , , LM5141 , UCC28700 Hi Team,
I want to realize PMP20345( http://www.ti.com/lit/df/tidrul7/tidrul7.pdf ) system using LM5141-Q1. This is because the LM5141 is better Iq and high frequency operation…