Part Number: UCC28740-Q1 Other Parts Discussed in Thread: UCC28740 Hi team,
My customer uses UCC28740-Q1 and they want to enable and disable this circuit with a MCU GPIO(like EN pin on other device). However, UCC28740-Q1 has no EN pin.
Question: …
Part Number: UCC28740-Q1 Other Parts Discussed in Thread: UCC28740 , TINA-TI , UCC28730 Hi TI,
I am currently try to simulate a flyback converter based on the UCC28740 isolated flyback controller. While I have accessed the SIMPLIS model provided on…
Part Number: UCC28740-Q1 Tool/software: Hi Team
Customer is using UCC28740Q1 to design a 100W flyback power.
They found that there were two different work conditions when it enters constant current mode, and the constant current level would be higher…
Part Number: UCC28740-Q1 Tool/software: Hello
We are planning to use, UCC28740QDRQ1 and UCC28730QDRQ1 in our design, But we need it to operate over a temperature range of -55 to 150degC . But as per datasheet recommended operating temp is given as …
Part Number: UCC28740-Q1 Tool/software: Hi Team
If the following turn on threshold voltage rang considers the temperature change drift? or it is typical value at 25℃?
Part Number: UCC28740-Q1 Other Parts Discussed in Thread: UCC28740
Tool/software:
Dear TI Support Team,
I am currently working with the UCC28740-Q1 in my application and have encountered an issue. I applied 24V to the VDD pin of the IC, but I observed…
Part Number: UCC28740-Q1 I want to design a two switch flyback (400V-15V 1.5A).I have come across the IC UCC28740-Q1.But the maximum switching frequency of this IC is found to be 100Khz.We need a bit higher swicthing frequency.Could you suggest any alternate…
Part Number: UCC28740-Q1 Other Parts Discussed in Thread: UCC28730-Q1 , UCC28730 , UCC28740 Tool/software: Hi,
I am planning to use UCC28740-Q1 for flyback application with 40V - 1500V input and 12V output.
Can I use voltage feedback from auxiliary…
Part Number: UCC28740-Q1 Tool/software: I am using the UCC28740-Q1 to design a flyback.
This IC includes the HV pin which provide the path to charge the VDD of IC during start up. However, after charging the VDD pin to turn-on level (CH2 reached 21V…