Part Number: UCC2891 hi ,
i need some information about UCC2891.I am using that chip into 500 watts dc to dc application.its able handle 500 watts or not ?
INPUT RANGE=60-84VDC,
INPUT CURRENT=8.3A,
OUTPUT VOLTAGE=14
OUTPUT CURRENT=35A
POWER…
Part Number: UCC2891 Other Parts Discussed in Thread: TINA-TI Hi Experts,
I am looking to design a 300W DCDC converter with the following specs:
Vin = 70VDC- 125VDC
Vout = 9VDC-16VDC, 14.4VDC nominal.
pout = 300W
isolated topology
I…
Part Number: UCC2891 Other Parts Discussed in Thread: UCC28C50 , UCC2800 , LM5025A , LM5026 Hello guys,
One of my customers is considering using UCC2891 for their new products. They want to design a isolated power supply which has Vin=9~36V(DC), Vo…
Part Number: UCC2891 Other Parts Discussed in Thread: UCC2894 , , UCC2897A , UCC28951 Hello teams,
I would like to design a offline power supply using forward converter topology.
The specifications are as follows
Input voltage: 280V to 330V
Output…
Part Number: UCC2891 Hi TI,
I read a post in relation to the magnetizing inductance of the transformer used in the SLUA303 technical note, PA0810, and I still have a doubt, because the transformer manufacturer (Pulse eng) specifies a Lmag=345uH, and…
Hi, Rock
Thanks for your interest in TI here. I will be happy to route your request into the appropriate team to support. Please note the team that supports this device is in the US so they will have a delayed response due to the US holiday. Please…
Part Number: UCC2891 Other Parts Discussed in Thread: TINA-TI I am using IC UCC2891D need current sharing method
how to use current sharing techniques
please provide detailed design process and understanding PMP2214 PM2214.pdf
Part Number: UCC2891 Other Parts Discussed in Thread: UCC2897A Hello E2E,
I know this device has 13.5V threshold for startup and it stop when the VDD over threshold. However, this characteristic detail is not find on datasheet. Does the 13.5V threshold…
Part Number: UCC2891 Other Parts Discussed in Thread: , , UCC2892 , UCC2893 , UCC2894 Hello!
Can I use your UCC2891X with Secondary-side regulation?
I do not have auxiliary winding and would like to power the IC from the primary winding and use an…
Part Number: UCC2891 I have my voltage input from 19.2 to 148v and I want an output of 5v@12A, 15v@3A and -15v@0.5A. I am thinking to make the active clamp forward converter. Will UCC2891 works in this input range? If any reference design available please…