Part Number: UCC28911 Hi Team,
I want to confirm if there is any small package of UCC28911 will be pushed such as DYY, DDF, DDC... And could you share the small package information and RTM time if we have. Thanks.
Best Regards,
Ryker
Part Number: UCC28911 Other Parts Discussed in Thread: UCC28710 , UCC28730 , PMP15002 , PMP Dear Team,
Do we have AC to DC Fly back topology regulator chipset to support 230VAc to 5V@3.5-4A.
Kindly suggest the best suitable part.
Thanks & Regards,
…
Part Number: UCC28911 Other Parts Discussed in Thread: UCC28750 , UCC28700 , UCC28710 , PMP30026 hello actually we use a secondary isolated flyback solution and we are looking renew our old design :
target : 10 to 12W output power, 230VAC 50Hz , 12 years…
Part Number: UCC28911 hello
I am designing a 8W isolated power supply to be integrated into an IOT design
I tryed to be inspired by the ref design of the UCC28911
please can you help me to optimize the size and validate my schematics and layout
best …
Part Number: UCC28911 Hi team,
UCC28911's datasheet mentioned that the maximum power UCC28911 can support is 12w, shown as below. And my customer wants to know the maximum power of UCC28911 under 90℃ and no wind condition. Could you pls help to answer…
Part Number: UCC28911
Hi Team,
Our customer is looking for a reference design of UCC28911 with the following specifications:
Input Aux Voltage Range : 50V to 300V AC
Operating Frequency : 45 to 65 Hz
Required Output Voltage : 3.3V DC
Required Output…
Part Number: UCC28911 Other Parts Discussed in Thread: UCC28C45 Hi Team,
This is a follow up inquiry to the E2E post below.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1236904/ucc28911-operating-voltage…
Part Number: UCC28911 Hi All,
I have a question about the output voltage of UCC28911.
I want to input 280V DC and output 54V DC, but according to WEBENCH, the maximum VOUT is 25V.
Is it possible to output 54V with UCC28911?
Best Regards, Ishiwata
Part Number: UCC28911 Hello, I use the UCC28911 as shown in the schematic, but it only works if the GND pin of the controller is connected to PE via a capacitor. The VS voltage at a successful start is shown in figure 2 and 3. A failed startup is shown…
Part Number: UCC28910 Other Parts Discussed in Thread: UCC28911 , , UCC28881 Hi Team
Can you provide the difference between UCC28910 and UCC28911? I only see the maximum power difference that can be handled, is there anything else? THX