Part Number: UCC3895 Other Parts Discussed in Thread: UCC28951 , , UCC2895 , UCC28950 , Greetings,
At least one section in this datasheet seems to have been lifted directly from the datasheet for the UCC28951 and does not apply to the UCC3895.
Specifically…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC2895-Q1 , UCC28950-Q1 , UCC2895 , UCC21520-Q1 , UCC21710-Q1 , UCC21530-Q1 Hi team
My customer wants to configure the system with the specifications below.
Input voltage : 800V
Output power : 24V…
Hello,
I gave this some thought last week and I don't believe this slope compensation circuit is that good. I would recommend using a high instead. divider off of CT instead.
1. Remove Q1 and Connect R1 to CT.
2. Disconnect R2 from CST and connect…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28950-Q1 , UCC2895-Q1 , UCC28951 Hello
Can I use UCC28951-Q1 for larger input voltage range ( 310 Vdc to 410 Vdc ) for developing DC-DC converter ?
If not what is the range of input voltage for…
Part Number: UCC25600 Other Parts Discussed in Thread: UCC28019A , TL431 , UCC28951 , UCC28950 , UCC2895 , UCC28951-Q1 , UCC28950-Q1 , PMP2187 , LM5035 , TL494 , UCC21520 , UCC2818
Dear All,
i selected the UCC25600 for a 400 W resonant converter.
the problem is…
Hi Stephan
The minimum switching frequency of the UCC2895 device is about 90kHz. Based on eq 2 in the DS and CT = 880pF and RT = 120kOhms (100pF < CT < 880pF and 40k < RT < 120k - bottom of page 11) .
This device is widely used and is often…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: TINA-TI , UCC28951 , UCC28950 , LM5046 , LM5045 , UCC2895 , UCC3895 , UCC1895 Tool/software: TINA-TI or Spice Models Hello,
I am trying to design a isolated DC DC boost converter with the following specs…
Other Parts Discussed in Thread: UCC3895 , UCC21520 , UCC2895 , UCC28951-Q1 , UCC28950 Hello All,
I have a question abouzt the UCC3595. We using it at our 5kW Power supply and it work in Voltage Mode (nor current feedback for the Ramp, but at moment I also…
Hi Lauren
You are correct, but there are some other things to consider.
The hiccup procedure will stop and normal operation resume if the ILIM condition is removed before the SS capacitor has been discharged to the 3.6V threshold.
The hiccup can be prevented…