Hi Rajesh,
Below are my responses to your query
rajesh Gudimani said: Is UCC28951 suitable for replacing ISL6754 in this application?
Yes, UCC28951 is functionally suitable as a replacement for ISL6754. Both are phase shifted full bridge (PSFB)…
Part Number: UCC28951-Q1 Dear TI team,
We are trying to simulate UCC28951-Q1 in LT Spice simulation but the simulation is not supporting the part number. Please help.
BR,
Abhiram
Part Number: UCC28951-Q1 HI,
PSFB Transformer is needed to be gapped in voltage/current mode in order to eliminate primary ZVS choke in ultra small size design?
Thanks
Regards
Andrew
Part Number: UCC28951-Q1 My Requirement is as below. Vin: - 70VDC ~ 150VDC Iin: - 20A Vout:- 420VDC Iout: - 5A Can i use PSFB topology to design this requirement power converter?? can i Used UCC28951-Q1 IC for this design??
Part Number: UCC28951-Q1 Tool/software: Hi, Can I use this IC UCC28951-Q1 for input 390VDC to 410VDC and output 25VDC to 120VDC at 500W constant output power?
If yes, how to manage duty cycle and transformer ratio. Please provide a solution.
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC29002 , UCC28950
I am working on a PSFB topology with the following specifications:
Input: 750 V DC
Output: 55 V DC
Power: :6.5 kW
Output current: 140 A (steady state), up to 250…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 Tool/software: Hello,
I am trying to design an isolated DC-DC converter with the following specifications:
Vin: 16-90 Vdc
Vout: 48 Vdc
Iout max: 30A
Using the TI Webench…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 Tool/software: Dear Sir,
I am currently designing a DC-DC converter using the PSFB configuration, with an input voltage range of 16.8V to 90V and an output of 48V at 30A. I require both…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 , PMP8740 Tool/software: I've following questions related to HV-LV converter: 1. In TIDA-020031, how it is ensured that LV battery is charged in cc cv mode?
2. In EV architecture the…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 , Tool/software: Dear Sir,
We are unable to check current sense current using KEYSIGHT InfiniVision MSOX3024T oscilloscope with High Voltage probe, Can you advise how to do that for…