Part Number: UCC2897A Hello,
I have designed a Forward converter using the UCC2897A and the transformer WURTH 750341138 I am encountering some issues with Vref and globally i have difficulties to undertsand why this circuit isn't working. The complete…
Part Number: UCC2897A Other Parts Discussed in Thread: LM5026 , , UCC24612 Hello TI experts:
Input: 36~75V
Output: 12V 72V
The design is expected to use UCC2897A (Active Clamp forward) at 350kHz.
Would you recommend using UCC24612 as the SR IC?
Or do…
Part Number: UCC2897A Other Parts Discussed in Thread: PMP8861 Hello TI Support Team,
I am designing an isolated DC-DC converter using the UCC2897A controller, based on the PMP8861 reference design. The converter operates correctly over the full input…
Part Number: UCC2897A Other Parts Discussed in Thread: UCC28C43 I'm considering designing a ZVS flyback converter based on the UCC2897A. I'm looking for low EMI, hence this choice.
General assumptions:
Vin = 24VDC +-10% Vo = 19V Io = 1.2A Galvanic…
Other Parts Discussed in Thread: UCC2897A , PMP8861 We are designing an active clamp forward converter using UCC2897A and need your technical guidance regarding pulse skipping operation at light load / no load condition .
The converter details are as…
Part Number: UCC2897A Other Parts Discussed in Thread: PMP8861 , , PMP Hi Experts,
Posting on customers behalf. Please see details below:
I have developed an isolated DC-DC converter based on the PMP8861 reference design.
Converter Specifications…
Part Number: UCC2897A Other Parts Discussed in Thread: UCC2892 , I have a P-CH active clamp forward design that I was going to implement with the UCC2892 until I noticed the UCC2897A. What are the pros and cons of using the UCC2897A over the UCC2892?…
Part Number: UCC2897A How to sync a 10 UCC2897A CIRCUITS configured as forward converters with an external sync signal. All my controllers are set to operate at 325kc. can u suggest some scheme. All shall be cofiguered as slave only.
Part Number: UCC2897A
Hi, I am simulation the IC in simmetrix. Secondary voltage is regulated as required.But,i see,Gate pulses toggling two to four times before actuall yturned off in simulation as shown below (green). AUX gate pulses is ok.CS voltage…
Part Number: UCC2897A Hi Team,
we are using UCC2897A Advanced Current-Mode Active-Clamp PWM Controller to genrate 12V from 54V DC input. We could see Vout is only 3.3V against the actual 12V output.
On further analysis we identified VCC_OUT supply…