Part Number: UCC28C41
Input Voltage: 100-240V, 50-60 Hz that converted in 400V DC
O/P Volage:24V
Output Power:200W
Hi all,
I will start working on design and development of a Power supply, with a continuous output power of 140W and peak power of 200W…
Part Number: UCC28C41-Q1 Tool/software: Hi team,
I would like to confrim with you that if UCC28C41-Q1 have the function to enter sleep mode to achieve lower power dissipation when it doesn't need to work. And if it can, how do we set the chip? And how…
Part Number: UCC28C41 Other Parts Discussed in Thread: TLV431A , TL431 Hi,
My customer used UCC28C41 to design a flyback with 3.3V/100mA for MUC VCC, they disable the 15V output circuit for the test.
I refer to the spec for voltage mode setup to add 2N222…
Part Number: UCC28C41 Hi Team
When using UCC28C41, cusotmer want to know
1.during normal operation, what is the approximate temperature difference between the UCC28C41DR junction to upper surface case?
2. Is there any corresponding application documents…
Part Number: UCC28C41-Q1 Hi team,
Customer would like to know whether we have p2p product of UCC28C4X-Q1 with lower UVLO (<6.5V) ? Or if there's work around method of external circuit to reduce UVLO value?
Thanks,
Scarlett
Part Number: UCC28C41-Q1 Other Parts Discussed in Thread: UCC28C40-Q1 , UCC28C41 Hi team,
I'd like to check my understanding about the difference between UCC28C41-Q1 and UCC28C40-Q1. UCC28C41-Q1 can only be operated with input from LV(12V battery as an…
Part Number: UCC28C41 Dear TI,
I am designing a SMPS by using controller UCC28C41. I am not able to do simulation of my SMPS design in Altium, by using the model file which is available in TI website.
For your information please find my error screen shot…
Part Number: UCC28C41-Q1 Other Parts Discussed in Thread: UCC28C41 hello,
I want know the minimum on time of UCC28C41. Because the I find the drive of UCC28C41 at high voltage and Light load have a fixed turn-on time (73ns). Therefore, I want to know why…
Hi,
The device typical Dmax is 50%, so the datasheet does not guarantee max Dmax not exceeding 50%.
You can consider other devices such UCC28C41, UCC28C44, or UCC28C45, these devices max Dmax guarantee not exceeding 50%.
Part Number: UCC28C41 Hello guys,
One of my customers is evaluating UCC28C41 on their own board using like Figure 31, Typical Application Design Schematic in the device datasheet(SLUS458G).
The device evaluation is going well. But they want to add a short…