Part Number: UCC28C41 Other Parts Discussed in Thread: TLV431A , TL431 Hi,
My customer used UCC28C41 to design a flyback with 3.3V/100mA for MUC VCC, they disable the 15V output circuit for the test.
I refer to the spec for voltage mode setup to add…
Part Number: UCC28C41 Hi Team
When using UCC28C41, cusotmer want to know
1.during normal operation, what is the approximate temperature difference between the UCC28C41DR junction to upper surface case?
2. Is there any corresponding application documents…
Part Number: UCC28C41-Q1 Other Parts Discussed in Thread: UCC28C41 hello,
I want know the minimum on time of UCC28C41. Because the I find the drive of UCC28C41 at high voltage and Light load have a fixed turn-on time (73ns). Therefore, I want to know…
Part Number: UCC28C41 Hello guys,
One of my customers is evaluating UCC28C41 on their own board using like Figure 31, Typical Application Design Schematic in the device datasheet(SLUS458G).
The device evaluation is going well. But they want to add…
Part Number: UCC28C41-Q1 Hi team,
Customer would like to know whether we have p2p product of UCC28C4X-Q1 with lower UVLO (<6.5V) ? Or if there's work around method of external circuit to reduce UVLO value?
Thanks,
Scarlett
Part Number: UCC28C41 Hi team,
UCC28C41 has a comp pin for EA output. In datasheet, it is current limit internally, could you share the value of the limit point? or maybe a curve can show the limit performance?
Thanks
Michael
Hi Vijay,
If you want to use the PSpice model for the device in Altium, please download the unencrypted PSpice model from the product folder. You will then have to follow the Altium instructions for how to install a PSpice model. You will still have…
Hi Cao,
Both of UCC28C41 and 28C40 can support HV input applications.
For duty cycle limitation . It only related to input voltage range , for narrow range input , the 50% max. duty cycle can meet output regulation and it can brings some benefits…
Hi Abhilash,
I have tested your circuit in TINA. It runs good.
Please see below simulation model and simulation results. and I also attached simulation model for your testing.
UCC28C41_STEADY.TSC
Regards,
Teng