Part Number: UCC28C41
Hi all,
I am testing the above boost converter with input of 15V and output should be 20V. But I am getting 17.2V only at output without load. Please help me to fix the issue. Feedback resistors values are also given above.
Thanks…
Part Number: UCC28C41 Hi all,
I tested with load also (0.5A). But still voltage is still reduced. that means
with load:
Vin=15V, ILOAD=0.5A
Vout=16V
Without load:
Vin=15V
Vout=17.5V
I probed the Vref pin. There are noises coupled at Vref pin so that…
Part Number: UCC28C41-Q1 Other Parts Discussed in Thread: TIDA-01505 , Hello all,
in the following TI presentation is mentioned a TIDA-01505 design with a UCC28C41-Q1 to convert 1000V down to 15V.
I can't find this reference design anywhere, could you help…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: LM34966-Q1 , UCC28C41-Q1 , LM5156 Dear team,
My customer plans to use our device as flyback controller(Primary-Side Regulated).
1. Our device doesn't have SCP/short circuit protection, do we have any…
Hi,
Yes, the die is the same between UCC38C41 and UCC28C1. At production, screen out UCC28C41 on wider temperature range. Then test UCC38C41 on narrow temperature range. But there are no tests for UCC28C41 with temperature range between 70C and 80C.
Hi,
It looks even better you can use UCC28C41 transient ref design to make simulation.. UCC28C44 has only difference on UVLO compared to UCC28C41. Actually UCC28C44 model is changed from UCC28C41 only on UVLO. These models have unencrypted version so…
Part Number: UCC2894 Other Parts Discussed in Thread: UCC28C41 Hello,
Please let me know about start threshold voltage. I'd like to input 12-V for Vdd, this device need to input more than 13.5-V at start up. Why this device needs this condition?
Regards…
Hi SAIKIRAN
You can use UCC28C41 module for simulation. Thank you.
https://www.ti.com/product/UCC28C41?keyMatch=UCC28C41&tisearch=Search-EN-everything&usecase=GPN#design-development