Part Number: UCC28C42-Q1 Hello Team,
i have a query related to UCC28C42-Q1. There is some information reletad in electrical characteristics which i wanted to confirm.
In the PWM duty cycle, where VFB > 2.6 , then output of the ASIC duty cycle is 0 percent…
Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: LMV431 , TL431 , UCC28C42 Hi Team,
We would like to ask your help regarding the customer's inquiry below.
When I design the UCC28C42QDRQ1 with Webench the adjustable precision shunt regulator…
Part Number: UCC28C42-Q1 Hello TI Team,
I wonder if it is possible to use the UCC28C42-Q1 and its internal current control loop to control the buck converter as a constant current source. Is such application is possible. Providing current feedback signal…
Part Number: UCC28950 Other Parts Discussed in Thread: UCC28C42-Q1 Tool/software: Hello Ti Team,
Actually my application is two switch forward converter with secondary side synchronous rectification.
First option:
Do we have any single TI controll…
Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: PMP10833 Hi Teng,
Can you please help me for reviewing the schematic attached? EFI_REGULATOR_BUCK_Schematic_VER_0.1_03Feb2020.pdf
Please review the buck converter in detail along with the component…
Maor,
The no load power consumption of 5mW is difficult. Low, no load power consumption is a feature you see with some off-line flyback controllers used in applications such as AC/DC adaptors. At VIN=12V, features targeting low, no load power consumption…
Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: UCC28C42 , LM5118 , PMP10833
Hi,
Can any one help me for reviewing the schematic attached? 5758.EFI Regulator.pdf
It is a design with buck and buck-boost converters using UCC28C42 PWM controller and…
Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: UCC28C42 , PMP10833 Hi,
For a flyback converter with UCC28C42 IC designed for the input range of 30-212VAC and output of 14VDC/6A, What will be the output voltage for the following inputs?
1. Vin…
Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: UCC28C42 Hi,
I have to design a power supply for a lawn mower system, which is taking power from alternator directly and converting it to the required DC power rails. There is no battery in the…