Part Number: UCC28C50-Q1
Hi,
In my flyback converter, I am facing an issue with the startup circuit. The converter is a working and tested design; however, the startup circuit is not functioning, and we currently need to provide an external supply…
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: UCC28C50 Tool/software: I am using the UCC28C50-Q1 in the Flyback circuit, while in low load, I see that PWM of the controller is skipping some cycles here and there.
There is nothing in the…
Hi Yajush,
Yajush Sihag said: Could you please help me identify which components in the schematic could cause the IC to stop generating gate pulses under these conditions?
Seems like COMP is not able to hold above ground for a long time. You can also…
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: TL431 Hi,
For 90W flyback converter
Vin = 100-160 VDC
Vo = 15V at 6A
Fsw = 100 kHz
There slight differenct in webench power designer and datasheet schematic in case of slop compensation…
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: TL431 , TINA-TI Hi,
I am designing a flyback with this IC with SSR. Webench designer suggested me following circuit
Webench designer - webench.ti.com/.../43
Should i go with this circuit…
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: UCC28C50 , Starting from these Flyback PSR and SSR Webench designs: webench.ti.com/.../SDP.cgi webench.ti.com/.../SDP.cgi
I've just buld up 2 build up 2 circuits using a custom multiout transformer…
Part Number: UCC28C50-Q1 Tool/software: Dear TI Team,
Can you provide suitable topology for below application.
Input Voltage Range 9 to 60V
Nominal Input 28 V
Output voltage 1: +15V, 7 A
Output voltage 2 - 15V, 0.5 A
Total power is around…
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: UCC28C50 Hi
we are building a ± 12V @ 4A output where input is 230VAC 50Hz is it possible to build the dual supply using single IC? if there is a reference design please let me know.
Dhaval Ravat said: The waveform of the voltage drop across the Aux diode when a Schottky diode is installed:
Dhaval Ravat said: The waveform of the voltage drop across the Aux diode when a PN diode is installed:
Dhaval Ravat said: Peak voltage…
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: LM5180 , LM25183 Hi Team,
I'm looking for designing an isolated bi-polar power supply with fly-back topology for my Mosfet Gate driver circuit. I'm little confused on selecting right controller…