Hi,
Please look into UCC28C53-Q1- which is a pin-pin replacement with low operating current.
Please let me know if you have more questions. Else if you feel that your question was answered, please click on "This resolved my issue" button.
Thanks…
Hello Sean,
Ok
But as discussed i will be using UCC28C53-Q1 controller, so UCC28C53-Q1 controller need minimum of 10V to 12V for VDD supply which to give UCC28C53-Q1 controller output (OUT) of 12V.
I understood one of your solution recommendation…
Part Number: UCC28C55 Other Parts Discussed in Thread: UCC28C43 , UCC28C53 Hi
I have design DC DC Power Supply.
Input Voltage 15VDC to 60VDC / 80VDC to 400VDC
Output Voltage-5V/2A
Line/Load Regulation-1%
Efficiency - 85% or above
I have select…
Other Parts Discussed in Thread: UCC28C53 , UC2843 , UCC28C43 Hello,
Can you please suggest suitable Boost converter to meet the following requirements?
Vin range : +20VDC to +140VDC
Vout Output voltage : +70VDC
Output current : 0.9A
We want…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: UCC28951 , UCC25600 , UCC2897A
Tool/software:
Dear team,
My customer would like to design power supply with below specification.
- Input : 30V ~ 60V(Typ. 48V)
- output : 24V / 10A, isolated…
Other Parts Discussed in Thread: UCC28C43 , UCC28C53 , UCC28C55 , TIDA-01505 Hi
I have design DC DC Power Supply in automations Card.
Input- 15V to 60V DC / 80Vto 400VDC
Output -5V upto 2A
Line/Load Regulations-1%
Efficiency-above 85%
Please…
Part Number: UCC28C44 Other Parts Discussed in Thread: UCC28C41 , UCC28C43 , UCC28C53
Hi,
I created a booster circuit using UC28C43. It worked fine in Tina TI, but I cannot simulate in Pspice for TI. I tried swapping models with UCC28C41 and UCC28C43…
Part Number: UCC28C43 Other Parts Discussed in Thread: UCC28C53-Q1 , TIDA-01505 Tool/software: Hi TI,
For example, I plan to use UCC28C53-Q1 to design a wide voltage input power supply.
Input voltage range: 13Vdc ~ 400Vdc Output specification: 80V…
Part Number: UCC28C58 Other Parts Discussed in Thread: UCC28C43 , UCC28C53 Hello,
I am looking for support on Simulation of UCC28C58, I am using Pspice for Ti.
I am not seeing any output, does TI provide any reference simulation design of UCC28C58…